AM243x MCU+ SDK  12.01.00
ram.h File Reference

Go to the source code of this file.

Data Structures

struct  Ram_DevConfig
 
struct  Ram_Attrs
 
struct  Ram_Fxns
 Driver implementation callbacks. More...
 
struct  Ram_Config
 Ram driver configuration, these are filled by SysCfg based on the ram device that is selected. More...
 
struct  Ram_Params
 Parameters passed during RAM_open() More...
 

Typedefs

typedef void * Ram_Handle
 Handle to the RAM driver returned by Ram_open() More...
 
typedef struct Ram_Config_s Ram_Config
 Forward declaration of Ram_Config. More...
 
typedef struct Ram_Params_s Ram_Params
 Forward declaration of Ram_Params. More...
 
RAM driver implementation callbacks
typedef int32_t(* Ram_OpenFxn) (Ram_Config *config)
 Driver implementation to open a specific RAM driver. More...
 
typedef void(* Ram_CloseFxn) (Ram_Config *config)
 Driver implementation to close a specific RAM driver. More...
 
typedef int32_t(* Ram_ReadFxn) (Ram_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)
 Driver implementation to read from RAM using a specific RAM driver. More...
 
typedef int32_t(* Ram_WriteFxn) (Ram_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)
 Driver implementation to write to RAM using specific RAM driver. More...
 
typedef int32_t(* Ram_quirksFxn) (Ram_Config *config)
 Ram device config. This will be part of the ram config, so has to be filled by sysconfig or otherwise before invoking Ram_open. More...
 
typedef int32_t(* Ram_custProtocolFxn) (Ram_Config *config)
 User implementation of a custom function to configure RAM to operate in a specific protocol. More...
 

Functions

Ram_Attrs * Ram_getAttrs (uint32_t instanceId)
 
Ram_Handle Ram_open (uint32_t instanceId, Ram_Params *params)
 Open RAM driver. More...
 
void Ram_close (Ram_Handle handle)
 Close RAM driver. More...
 
int32_t Ram_write (Ram_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
 Write to RAM device. More...
 
int32_t Ram_read (Ram_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
 Read data from RAM device. More...