AM243x MCU+ SDK  12.01.00
mmcsd_lld.h
Go to the documentation of this file.
1 /*
2  * Copyright (C) 2024-2025 Texas Instruments Incorporated
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
54 #ifndef MMCSD_LLD_H_
55 #define MMCSD_LLD_H_
56 
57 /* ========================================================================== */
58 /* Include Files */
59 /* ========================================================================== */
60 
61 #ifdef __cplusplus
62 extern "C" {
63 #endif
64 
65 #include <stdint.h>
66 #include <stdbool.h>
67 #include <stdlib.h>
68 #include <stddef.h>
69 #include <string.h>
70 #include <drivers/hw_include/cslr.h>
71 #include <drivers/hw_include/cslr64.h>
72 #include <drivers/hw_include/hw_types.h>
73 #include <drivers/hw_include/cslr_mmcsd.h>
74 #include <drivers/mmcsd/v0/cslr_mmcsd.h>
75 
76 /* ========================================================================== */
77 /* Macros & Typedefs */
78 /* ========================================================================== */
79 
87 #define MMCSD_STS_SUCCESS ((int32_t) 0)
88 
90 #define MMCSD_STS_ERR ((int32_t)-1)
91 
93 #define MMCSD_STS_ERR_TIMEOUT ((int32_t)-2)
94 
95 #define MMCSD_STS_ERR_INVALID_PARAM ((int32_t)-3)
96 
97 #define MMCSD_STS_ERR_BUSY ((int32_t)-4)
98 
99 #define MMCSD_STS_ERR_CARD_NOT_FOUND ((int32_t)-5)
100 
101 #define MMCSD_STS_ERR_CARD_UNUSEABLE ((int32_t)-6)
102 
103 #define MMCSD_STS_ERR_CARD_UNLOCK_FAIL ((int32_t)-7)
104 
115 #define MMCSD_NO_WAIT ((uint32_t)0)
116 
118 #define MMCSD_WAIT_FOREVER ((uint32_t)-1)
119 
130 #define MMCSD_STATE_RESET ((uint8_t) 0U)
131 
133 #define MMCSD_STATE_IDLE ((uint8_t) 1U)
134 
136 #define MMCSD_STATE_BUSY ((uint8_t) 2U)
137 
139 #define MMCSD_STATE_ERROR ((uint8_t) 3U)
140 
150 #define MMCSD_XFER_IDLE_STATE ((uint8_t) 0U)
151 
152 #define MMCSD_XFER_CMD_STATE ((uint8_t) 1U)
153 
154 #define MMCSD_XFER_WRITE_STATE ((uint8_t) 2U)
155 
156 #define MMCSD_XFER_READ_STATE ((uint8_t) 3U)
157 
166 #define MMCSD_SLOT_TYPE_VAL_REMOVABLE ((uint8_t) 0x0U)
167 #define MMCSD_SLOT_TYPE_VAL_EMBEDDED ((uint8_t) 0x1U)
168 #define MMCSD_SLOT_TYPE_VAL_SHARED ((uint8_t) 0x2U)
169 
178 #define MMCSD_CARD_TYPE_SD ((uint32_t) 0U)
179 #define MMCSD_CARD_TYPE_EMMC ((uint32_t) 2U)
180 #define MMCSD_CARD_TYPE_NO_DEVICE ((uint32_t) 3U)
181 
190 #define MMCSD_PHY_TYPE_HW_PHY ((uint32_t) 0U)
191 #define MMCSD_PHY_TYPE_SW_PHY ((uint32_t) 1U)
192 #define MMCSD_PHY_TYPE_NO_PHY ((uint32_t) 2U)
193 
202 #define MMCSD_BUS_WIDTH_4BIT ((uint32_t) 0x4U)
203 #define MMCSD_BUS_WIDTH_8BIT ((uint32_t) 0x8U)
204 #define MMCSD_BUS_WIDTH_1BIT ((uint32_t) 0x1U)
205 
214 #define MMCSD_PHY_TUNING_TYPE_AUTO ((uint32_t) 0U)
215 #define MMCSD_PHY_TUNING_TYPE_MANUAL ((uint32_t) 1U)
216 
225 #define MMCSD_SD_MODE_HS ((uint32_t) 10U)
226 #define MMCSD_SD_MODE_DS ((uint32_t) 11U)
227 #define MMCSD_SD_MODE_SDR12 ((uint32_t) 12U)
228 #define MMCSD_SD_MODE_SDR25 ((uint32_t) 13U)
229 #define MMCSD_SD_MODE_SDR50 ((uint32_t) 14U)
230 #define MMCSD_SD_MODE_DDR50 ((uint32_t) 15U)
231 #define MMCSD_SD_MODE_SDR104 ((uint32_t) 16U)
232 
241 #define MMCSD_MMC_MODE_SDR25 ((uint32_t) 20U)
242 #define MMCSD_MMC_MODE_SDR50 ((uint32_t) 21U)
243 #define MMCSD_MMC_MODE_HS200 ((uint32_t) 23U)
244 
247 /* ========================================================================== */
248 /* Function Pointers Declarations */
249 /* ========================================================================== */
250 
258 typedef void (*MMCSD_lld_transferCompleteCallback) (void *args,
259  int32_t xferStatus);
260 
261 /* ========================================================================== */
262 /* Structure Declarations */
263 /* ========================================================================== */
264 
268 typedef struct {
269 
271  uint32_t ocr;
273  uint32_t rca;
275  uint16_t maxReadBlockLen;
279  char manuDate[9];
281  uint8_t manuID;
283  char productName[7];
285  uint8_t specVersion;
287  uint32_t blockCount;
289  uint8_t transferSpeed;
291  uint8_t supportedModes;
293  uint8_t eStrobeSupport;
295  uint8_t driveStrength;
297  bool isHC;
298 
300 
304 typedef struct {
305 
307  uint32_t ocr;
309  uint32_t rca;
311  uint16_t maxReadBlockLen;
315  char manuDate[9];
317  uint8_t manuID;
319  char productName[6];
321  uint8_t specVersion;
323  uint32_t blockCount;
325  uint8_t transferSpeed;
327  uint32_t isCmd23;
331  bool isHC;
332 
334 
342 typedef struct {
343 
345  uint32_t cmd;
347  uint32_t dir;
349  uint32_t arg;
351  uint8_t *dataBuf;
353  uint32_t blockSize;
355  uint32_t blockCount;
357  uint32_t autoCmdEn;
359  uint32_t enableDma;
361  uint32_t isTuning;
363  uint32_t response[4];
364 
366 
370 typedef struct {
371 
373  uint32_t ctrlBaseAddr;
375  uint32_t ssBaseAddr;
377  uint32_t inputClkFreq;
379  uint32_t cardType;
383  uint32_t uaBusSpeed;
386  uint32_t tuningType;
388  uint32_t intrNum;
390  uint32_t slotType;
392  uint32_t busWidth;
394  bool enableDma;
396  uint32_t phyType;
400  void *deviceData;
404  uint8_t *dataBuf;
405 
407 
408 
412 typedef struct {
413 
415  uint16_t cmdErrorStat;
417  uint16_t xferErrorStat;
419  uint8_t *dataBufIdx;
421  uint32_t dataBlockCount;
423  uint32_t dataBlockSize;
432  uint32_t setBusSpeed;
434  uint32_t setBusWidth;
436  uint8_t xferState;
438  uint8_t state;
442  void *args;
445 
447 
448 /* ========================================================================== */
449 /* API Function Declarations */
450 /* ========================================================================== */
451 
460 
469 
483 
494 int32_t MMCSD_lld_write_SD_Poll(MMCSDLLD_Handle handle, uint8_t *buf,
495  uint32_t startBlk, uint32_t numBlks);
496 
507 int32_t MMCSD_lld_read_SD_Poll(MMCSDLLD_Handle handle, uint8_t *buf,
508  uint32_t startBlk, uint32_t numBlks);
509 
520 int32_t MMCSD_lld_write_MMC_Poll(MMCSDLLD_Handle handle, uint8_t *buf,
521  uint32_t startBlk, uint32_t numBlks);
522 
533 int32_t MMCSD_lld_read_MMC_Poll(MMCSDLLD_Handle handle, uint8_t *buf,
534  uint32_t startBlk, uint32_t numBlks);
535 
546 int32_t MMCSD_lld_write_SD_Intr(MMCSDLLD_Handle handle, uint8_t *buf,
547  uint32_t startBlk, uint32_t numBlks);
548 
559 int32_t MMCSD_lld_read_SD_Intr(MMCSDLLD_Handle handle, uint8_t *buf,
560  uint32_t startBlk, uint32_t numBlks);
561 
572 int32_t MMCSD_lld_write_MMC_Intr(MMCSDLLD_Handle handle, uint8_t *buf,
573  uint32_t startBlk, uint32_t numBlks);
574 
585 int32_t MMCSD_lld_read_MMC_Intr(MMCSDLLD_Handle handle, uint8_t *buf,
586  uint32_t startBlk, uint32_t numBlks);
587 
598  uint32_t busSpeed, uint32_t busWidth);
599 
609  uint32_t busSpeed);
610 
620  uint32_t tuningType);
621 
635  uint32_t partitionNum);
636 
649 
650 /* ========================================================================== */
651 /* ISR Function Declarations */
652 /* ========================================================================== */
653 
660 void MMCSD_lld_Isr(void *args);
661 
662 #ifdef __cplusplus
663 }
664 #endif
665 
666 #endif /* MMCSD_LLD_H_ */
667 
MMCSDLLD_Object::setBusSpeed
uint32_t setBusSpeed
Definition: mmcsd_lld.h:432
MMCSDLLD_Object::dataBufIdx
uint8_t * dataBufIdx
Definition: mmcsd_lld.h:419
MMCSDLLD_InitObject::slotType
uint32_t slotType
Definition: mmcsd_lld.h:390
MMCSD_lld_read_SD_Poll
int32_t MMCSD_lld_read_SD_Poll(MMCSDLLD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
Function to perform block reads from the SD media in Polling Mode.
MMCSDLLD_InitObject::intrNum
uint32_t intrNum
Definition: mmcsd_lld.h:388
MMCSD_SdDeviceData::ocr
uint32_t ocr
Definition: mmcsd_lld.h:307
MMCSDLLD_InitObject::autoAssignMaxSpeed
bool autoAssignMaxSpeed
Definition: mmcsd_lld.h:381
MMCSD_SdDeviceData::manuID
uint8_t manuID
Definition: mmcsd_lld.h:317
MMCSDLLD_Object::transferCompleteCallback
MMCSD_lld_transferCompleteCallback transferCompleteCallback
Definition: mmcsd_lld.h:444
MMCSD_SdDeviceData::transferSpeed
uint8_t transferSpeed
Definition: mmcsd_lld.h:325
MMCSDLLD_InitObject::dataBuf
uint8_t * dataBuf
Definition: mmcsd_lld.h:404
MMCSD_EmmcDeviceData::blockCount
uint32_t blockCount
Definition: mmcsd_lld.h:287
MMCSDLLD_InitObject::enableDma
bool enableDma
Definition: mmcsd_lld.h:394
MMCSD_SdDeviceData
SD device properties.
Definition: mmcsd_lld.h:304
MMCSD_EmmcDeviceData::rca
uint32_t rca
Definition: mmcsd_lld.h:273
MMCSDLLD_Object::state
uint8_t state
Definition: mmcsd_lld.h:438
MMCSD_lld_enableBootPartition
int32_t MMCSD_lld_enableBootPartition(MMCSDLLD_Handle handle, uint32_t partitionNum)
Function to enable the boot partition given the media is eMMC.
MMCSD_lld_Isr
void MMCSD_lld_Isr(void *args)
This is the MMCSD Controller ISR and can be used as IRQ handler.
MMCSD_SdDeviceData::specVersion
uint8_t specVersion
Definition: mmcsd_lld.h:321
MMCSD_lld_read_MMC_Intr
int32_t MMCSD_lld_read_MMC_Intr(MMCSDLLD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
Function to perform block reads from the MMC media in Interrupt Mode.
MMCSDLLD_Object::setBusWidth
uint32_t setBusWidth
Definition: mmcsd_lld.h:434
MMCSDLLD_Transaction
MMCSDLLD Transaction.
Definition: mmcsd_lld.h:342
MMCSDLLD_InitObject::pllEnableSD
bool pllEnableSD
Definition: mmcsd_lld.h:398
MMCSDLLD_InitObject::tuningType
uint32_t tuningType
Definition: mmcsd_lld.h:386
MMCSDLLD_Transaction::arg
uint32_t arg
Definition: mmcsd_lld.h:349
MMCSDLLD_Object::xferErrorStat
uint16_t xferErrorStat
Definition: mmcsd_lld.h:417
MMCSD_SdDeviceData::maxReadBlockLen
uint16_t maxReadBlockLen
Definition: mmcsd_lld.h:311
MMCSDLLD_InitObject::ctrlBaseAddr
uint32_t ctrlBaseAddr
Definition: mmcsd_lld.h:373
MMCSD_lld_write_MMC_Intr
int32_t MMCSD_lld_write_MMC_Intr(MMCSDLLD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
Function to perform block writes to the MMC media in Interrupt Mode.
MMCSD_SdDeviceData::isHC
bool isHC
Definition: mmcsd_lld.h:331
MMCSD_lld_deInit
int32_t MMCSD_lld_deInit(MMCSDLLD_Handle handle)
This API De-Initializes the MMCSD instance.
MMCSDLLD_Transaction::autoCmdEn
uint32_t autoCmdEn
Definition: mmcsd_lld.h:357
MMCSD_lld_write_SD_Intr
int32_t MMCSD_lld_write_SD_Intr(MMCSDLLD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
Function to perform block writes to the SD media in Interrupt Mode.
MMCSDLLD_Object::currentTxn
MMCSDLLD_Transaction * currentTxn
Definition: mmcsd_lld.h:427
MMCSDLLD_InitObject
MMCSD Driver Initialization Object.
Definition: mmcsd_lld.h:370
MMCSD_EmmcDeviceData::eStrobeSupport
uint8_t eStrobeSupport
Definition: mmcsd_lld.h:293
MMCSD_EmmcDeviceData::manuID
uint8_t manuID
Definition: mmcsd_lld.h:281
MMCSD_SdDeviceData::isCmd23
uint32_t isCmd23
Definition: mmcsd_lld.h:327
MMCSD_EmmcDeviceData::specVersion
uint8_t specVersion
Definition: mmcsd_lld.h:285
MMCSD_EmmcDeviceData::ocr
uint32_t ocr
Definition: mmcsd_lld.h:271
MMCSDLLD_InitObject::cardType
uint32_t cardType
Definition: mmcsd_lld.h:379
MMCSDLLD_InitObject::ssBaseAddr
uint32_t ssBaseAddr
Definition: mmcsd_lld.h:375
MMCSD_lld_change_Bus_Config_MMC
int32_t MMCSD_lld_change_Bus_Config_MMC(MMCSDLLD_Handle handle, uint32_t busSpeed, uint32_t busWidth)
Function to reconfigure the bus Speed and Bus width of the bus for MMC.
MMCSDLLD_Object
MMCSD Driver Object.
Definition: mmcsd_lld.h:412
MMCSDLLD_Transaction::blockCount
uint32_t blockCount
Definition: mmcsd_lld.h:355
MMCSDLLD_InitHandle
struct MMCSDLLD_InitObject * MMCSDLLD_InitHandle
MMCSDLLD_Transaction::dataBuf
uint8_t * dataBuf
Definition: mmcsd_lld.h:351
MMCSD_lld_read_SD_Intr
int32_t MMCSD_lld_read_SD_Intr(MMCSDLLD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
Function to perform block reads from the SD media in Interrupt Mode.
MMCSD_SdDeviceData::rca
uint32_t rca
Definition: mmcsd_lld.h:309
MMCSD_lld_disableBootPartition
int32_t MMCSD_lld_disableBootPartition(MMCSDLLD_Handle handle)
This function disables the boot partition if the media is eMMC.
MMCSDLLD_Object::remainingBlockCount
uint32_t remainingBlockCount
Definition: mmcsd_lld.h:425
MMCSD_EmmcDeviceData::supportedModes
uint8_t supportedModes
Definition: mmcsd_lld.h:291
MMCSDLLD_Transaction::blockSize
uint32_t blockSize
Definition: mmcsd_lld.h:353
MMCSD_lld_write_SD_Poll
int32_t MMCSD_lld_write_SD_Poll(MMCSDLLD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
Function to perform block writes to the SD media in Polling Mode.
MMCSDLLD_Object::dataBlockCount
uint32_t dataBlockCount
Definition: mmcsd_lld.h:421
MMCSD_lld_read_MMC_Poll
int32_t MMCSD_lld_read_MMC_Poll(MMCSDLLD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
Function to perform block reads from the MMC media in Polling Mode.
MMCSD_lld_init
int32_t MMCSD_lld_init(MMCSDLLD_Handle handle)
This API Initializes the MMCSD instance.
MMCSD_EmmcDeviceData
eMMC device properties
Definition: mmcsd_lld.h:268
MMCSD_EmmcDeviceData::maxReadBlockLen
uint16_t maxReadBlockLen
Definition: mmcsd_lld.h:275
MMCSDLLD_InitObject::busWidth
uint32_t busWidth
Definition: mmcsd_lld.h:392
MMCSDLLD_Handle
struct MMCSDLLD_Object * MMCSDLLD_Handle
MMCSD_EmmcDeviceData::transferSpeed
uint8_t transferSpeed
Definition: mmcsd_lld.h:289
MMCSD_SdDeviceData::supportedDataWidths
uint32_t supportedDataWidths
Definition: mmcsd_lld.h:329
MMCSDLLD_Object::mmcsdTxn
MMCSDLLD_Transaction mmcsdTxn
Definition: mmcsd_lld.h:429
MMCSD_EmmcDeviceData::maxWriteBlockLen
uint16_t maxWriteBlockLen
Definition: mmcsd_lld.h:277
MMCSDLLD_Transaction::isTuning
uint32_t isTuning
Definition: mmcsd_lld.h:361
MMCSD_lld_change_Bus_Config_SD
int32_t MMCSD_lld_change_Bus_Config_SD(MMCSDLLD_Handle handle, uint32_t busSpeed)
Function to reconfigure the bus Speed and Bus width of the bus for MMC.
MMCSD_lld_getBlockSize
uint32_t MMCSD_lld_getBlockSize(MMCSDLLD_Handle handle)
This function returns the block size of the MMC/SD media connected to the MMCSD controller.
MMCSDLLD_InitObject::deviceData
void * deviceData
Definition: mmcsd_lld.h:400
MMCSDLLD_Transaction::dir
uint32_t dir
Definition: mmcsd_lld.h:347
MMCSD_lld_write_MMC_Poll
int32_t MMCSD_lld_write_MMC_Poll(MMCSDLLD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
Function to perform block writes to the MMC media in Polling Mode.
MMCSD_EmmcDeviceData::isHC
bool isHC
Definition: mmcsd_lld.h:297
MMCSDLLD_InitObject::phyType
uint32_t phyType
Definition: mmcsd_lld.h:396
MMCSDLLD_Object::dataBlockSize
uint32_t dataBlockSize
Definition: mmcsd_lld.h:423
MMCSD_SdDeviceData::blockCount
uint32_t blockCount
Definition: mmcsd_lld.h:323
MMCSDLLD_Object::initHandle
MMCSDLLD_InitHandle initHandle
Definition: mmcsd_lld.h:440
MMCSDLLD_Transaction::cmd
uint32_t cmd
Definition: mmcsd_lld.h:345
MMCSDLLD_Transaction::enableDma
uint32_t enableDma
Definition: mmcsd_lld.h:359
MMCSD_lld_transferCompleteCallback
void(* MMCSD_lld_transferCompleteCallback)(void *args, int32_t xferStatus)
The definition of a transfer completion callback function used by the MMCSD driver when used in Callb...
Definition: mmcsd_lld.h:258
MMCSDLLD_InitObject::inputClkFreq
uint32_t inputClkFreq
Definition: mmcsd_lld.h:377
MMCSDLLD_Object::args
void * args
Definition: mmcsd_lld.h:442
MMCSDLLD_Object::xferState
uint8_t xferState
Definition: mmcsd_lld.h:436
MMCSDLLD_Object::cmdErrorStat
uint16_t cmdErrorStat
Definition: mmcsd_lld.h:415
MMCSD_EmmcDeviceData::driveStrength
uint8_t driveStrength
Definition: mmcsd_lld.h:295
MMCSDLLD_InitObject::uaBusSpeed
uint32_t uaBusSpeed
Definition: mmcsd_lld.h:383
MMCSD_lld_change_Tuning_Type
int32_t MMCSD_lld_change_Tuning_Type(MMCSDLLD_Handle handle, uint32_t tuningType)
Function to reconfigure the bus Speed and Bus width of the bus for MMC.
MMCSD_SdDeviceData::maxWriteBlockLen
uint16_t maxWriteBlockLen
Definition: mmcsd_lld.h:313