AM243x MCU+ SDK  12.01.00
icssg.h File Reference

Introduction

This file contains the type definitions and helper macros for the ICSSG peripheral interface.

Go to the source code of this file.

Data Structures

struct  Icssg_TxTsEvtCbInfo
 Icssg TX timestamp event callback info structure. This is passed to application when TX timestamp is retrieved by ICSSG driver. More...
 
struct  IcssgMacPort_SetQueueCtPremptModeInArgs
 Input arguments for ICSSG_MACPORT_IOCTL_SET_QUEUE_CUT_THROUGH_PREEMPT_SELECT command. More...
 
struct  IcssgMacPort_ConfigSpecialFramePrioInArgs
 Input arguments for ICSSG_MACPORT_IOCTL_CONFIG_SPL_FRAME_PRIO command. More...
 
struct  IcssgMacPort_SetPortStateInArgs
 Input args for ICSSG_MACPORT_IOCTL_SET_PORT_STATE command. More...
 
struct  Icssg_SetAcceptFrameCheckInArgs
 Input args for ICSSG_MACPORT_IOCTL_SET_ACCEPT_FRAME_CHECK command. More...
 
struct  Icssg_MacAddr
 MAC address. More...
 
struct  IcssgMacPort_SetMacAddressInArgs
 Input args for ICSSG_MACPORT_IOCTL_SET_MACADDR command. More...
 
struct  Icssg_VlanFidParams
 VLAN FID entry parameters. More...
 
struct  Icssg_VlanFidEntry
 VLAN FID table entry. More...
 
struct  Icssg_FdbEntry
 FDB entry configuration. More...
 
struct  Icssg_HwFdbEntry
 HW FDB table entry. More...
 
struct  Icssg_FdbEntry_ReadSlotInArgs
 Input arguments for ICSSG_FDB_IOCTL_READ_SLOT_ENTRIES command. More...
 
struct  Icssg_FdbEntry_GetSlotOutArgs
 Output arguments for ICSSG_FDB_IOCTL_GET_SLOT_ENTRIES command. More...
 
struct  Icssg_DfltVlanCfg
 Default VLAN configuration. More...
 
struct  Icssg_MacPortDfltVlanCfgInArgs
 Input arguments for ICSSG_PER_IOCTL_VLAN_SET_MACPORT_DFLT_VID command. More...
 
struct  Icssg_IngressRateLim
 Input arguments for ICSSG_MACPORT_IOCTL_SET_INGRESS_RATE_LIM command. More...
 
struct  Icssg_IngressRateLim::FT_S
 
union  Icssg_IngressRateLim::FT_S::FT_U
 
struct  Icssg_IngressRateLim::FT_S::FT_U::FT1_CONFIG_S
 
struct  Icssg_IngressRateLim::FT_S::FT_U::FT3_CONFIG_S
 
struct  Icssg_custom_Fw
 ICSSG custom firmware. More...
 
struct  Icssg_FwPoolMem
 ICSSG buffer pool memories. More...
 
struct  Icssg_MdioLinkStateChangeInfo
 PHY link status change event information. More...
 
struct  Icssg_mdioLinkIntCfg
 
struct  Icssg_portLinkIntCfg
 
struct  Icssg_Cfg
 ICSSG peripheral configuration parameters. More...
 
struct  IcssgMacPort_Cfg
 ICSSG mac port configuration parameters. More...
 

Macros

#define ICSSG_CFG_DEFAULT_AGING_PERIOD_MS   (0x6FC23AC00)
 
#define ICSSG_IEP_DFLT_CYCLE_TIME_NSECS   (1000000U)
 
#define ICSSG_PUBLIC_IOCTL(x)
 Helper macro to create IOCTL commands for ICSSG per. More...
 
#define ICSSG_PORT_NUM   (3U)
 Number of supported ports (host port, physical ports 1 and 2). More...
 
#define ICSSG_MAC_PORT_MAX   (ICSSG_PORT_NUM - 1U)
 Maximum number of MAC ports per ICSSG instance. More...
 
#define ICSSG_PER_DUALMAC_PORT_MAX   (1U)
 Maximum number of MAC ports in a ICSSG peripheral in Dual-MAC mode. Note that each port in Dual-MAC is handled as a separate Enet peripheral. More...
 
#define ICSSG_PER_SWITCH_PORT_MAX   (ICSSG_MAC_PORT_MAX)
 Maximum number of MAC ports in a ICSSG peripheral in Switch mode. More...
 
#define ICSSG_INSTANCE_NUM   (2U)
 Number of supported icssg instances. More...
 
#define ICSSG_MAX_NUM_BUFFER_POOLS   (24U)
 Max number of buffer pools. More...
 
#define ICSSG_DUALMAC_TX_CH_NUM   (ENET_CFG_RM_TX_CH_MAX)
 Number of TX channels per slice in Dual-MAC mode. More...
 
#define ICSSG_DUALMAC_RX_FLOW_NUM   (ENET_CFG_RM_RX_CH_MAX / 2)
 Number of RX flows per slice in Dual-MAC mode. More...
 
#define ICSSG_SWITCH_TX_CH_NUM   (ENET_CFG_RM_TX_CH_MAX)
 Number of TX channels in Switch mode. More...
 
#define ICSSG_SWITCH_RX_FLOW_NUM   (ENET_CFG_RM_RX_CH_MAX)
 Number of RX flows in Switch mode. More...
 
#define ICSSG_DUALMAC_PORT_BUFFER_POOL_NUM   (0U)
 Number of port buffer pools required for Dual-MAC. More...
 
#define ICSSG_DUALMAC_HOST_EGRESS_QUEUE_NUM   (2U)
 Number of host egress queues required for Dual-MAC. More...
 
#define ICSSG_SWITCH_PORT_BUFFER_POOL_NUM   (8U)
 Number of port buffer pools required for Dual-MAC. This value can be modified if required from 1 to 8. More...
 
#define ICSSG_SWITCH_PORT_BUFFER_POOL_NUM_MAX   (8U)
 Maximum number of port buffer pools. This offset used for Host pool init config. More...
 
#define ICSSG_SWITCH_HOST_OWN_BUFFER_POOL_MAX_OFFSET   (16U)
 Maximum number of Host OWN buffer pools. This offset used for Host pool init config. More...
 
#define ICSSG_SWITCH_HOST_EGRESS_QUEUE_NUM   (2U)
 Number of host egress queues required for Dual-MAC. More...
 
#define ICSSG_HOST_EGRESS_BUFFER_PADDING   (2048U)
 Host egress queue padding size. More...
 
#define ICSSG_SCRATCH_BUFFER_SIZE   (ENET_UTILS_ALIGN((2048U), ICSSG_CACHELINE_ALIGNMENT))
 Size of the scratch buffer used for error frames and large frames. More...
 
#define ICSSG_RATE_SRC_SEL_FT1_MATCH0   (0U)
 
#define ICSSG_RATE_SRC_SEL_FT1_MATCH1   (1U)
 
#define ICSSG_RATE_SRC_SEL_FT1_MATCH2   (2U)
 
#define ICSSG_RATE_SRC_SEL_FT1_MATCH3   (3U)
 
#define ICSSG_RATE_SRC_SEL_FT1_MATCH4   (4U)
 
#define ICSSG_RATE_SRC_SEL_FT1_MATCH5   (5U)
 
#define ICSSG_RATE_SRC_SEL_FT1_MATCH6   (6U)
 
#define ICSSG_RATE_SRC_SEL_FT1_MATCH7   (7U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH0   (8U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH1   (9U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH2   (10U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH3   (11U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH4   (12U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH5   (13U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH6   (14U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH7   (15U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH8   (16U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH9   (17U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH10   (18U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH11   (19U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH12   (20U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH13   (21U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH14   (22U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH15   (23U)
 
#define ICSSG_RATE_SRC_SEL_FT_RX_UC   (24U)
 
#define ICSSG_RATE_SRC_SEL_FT_RX_MC   (25U)
 
#define ICSSG_RATE_SRC_SEL_FT_RX_BC   (26U)
 
#define ICSSG_RATE_SRC_SEL_FT_RX_SAV   (27U)
 
#define ICSSG_RATE_SRC_SEL_FT_RX_FWD   (28U)
 
#define ICSSG_RATE_SRC_SEL_FT_RX_RCV   (29U)
 
#define ICSSG_RATE_SRC_SEL_FT_RX_VLAN   (30U)
 
#define ICSSG_RATE_SRC_SEL_FT_RX_DA_P   (31U)
 
#define ICSSG_RATE_SRC_SEL_FT_RX_DA_I   (32U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW0   (33U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW1   (34U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW2   (35U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW3   (36U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW4   (37U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW5   (38U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW6   (39U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW7   (40U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW8   (41U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW9   (42U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW10   (43U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW11   (44U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW12   (45U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW13   (46U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW14   (47U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW15   (48U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH0   (0U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH1   (1U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH2   (2U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH3   (3U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH4   (4U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH5   (5U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH6   (6U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH7   (7U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH8   (8U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH9   (9U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH10   (10U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH11   (11U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH12   (12U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH13   (13U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH14   (14U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH15   (15U)
 
#define ICCSG_RX_CLASS_DATA_FT1_MATCH0   (16U)
 
#define ICCSG_RX_CLASS_DATA_FT1_MATCH1   (17U)
 
#define ICCSG_RX_CLASS_DATA_FT1_MATCH2   (18U)
 
#define ICCSG_RX_CLASS_DATA_FT1_MATCH3   (19U)
 
#define ICCSG_RX_CLASS_DATA_FT1_MATCH4   (20U)
 
#define ICCSG_RX_CLASS_DATA_FT1_MATCH5   (21U)
 
#define ICCSG_RX_CLASS_DATA_FT1_MATCH6   (22U)
 
#define ICCSG_RX_CLASS_DATA_FT1_MATCH7   (23U)
 
#define ICCSG_RX_CLASS_DATA_FT_RX_DA_I   (24U)
 
#define ICCSG_RX_CLASS_DATA_FT_RX_DA_P   (25U)
 
#define ICCSG_RX_CLASS_DATA_FT_RX_VLAN   (26U)
 
#define ICCSG_RX_CLASS_DATA_FT_RX_RCV   (27U)
 
#define ICCSG_RX_CLASS_DATA_FT_RX_FWD   (28U)
 
#define ICCSG_RX_CLASS_DATA_FT_RX_BC   (29U)
 
#define ICCSG_RX_CLASS_DATA_FT_RX_MC   (30U)
 
#define ICCSG_RX_CLASS_DATA_FT_RX_SAV   (31U)
 
#define ICSSG_TAS_MIN_CYCLE_TIME_NS   (1000000)
 Minimum cycle time supported by implementation (in ns). More...
 
#define ICSSG_TAS_MIN_WINDOW_DURATION_NS   (10000)
 Minimum TAS window duration supported by implementation (in ns). More...
 
ICSSG FDB entry fields.

#define ICSSG_FDB_ENTRY_P0_MEMBERSHIP   (ENET_BIT(0U))
 Host port membership. More...
 
#define ICSSG_FDB_ENTRY_P1_MEMBERSHIP   (ENET_BIT(1U))
 Physical port 1 membership. More...
 
#define ICSSG_FDB_ENTRY_P2_MEMBERSHIP   (ENET_BIT(2U))
 Physical port 2 membership. More...
 
#define ICSSG_FDB_ENTRY_AGEABLE   (ENET_BIT(3U))
 Ageable bit. More...
 
#define ICSSG_FDB_ENTRY_BLOCK   (ENET_BIT(4U))
 Block bit. More...
 
#define ICSSG_FDB_ENTRY_SECURE   (ENET_BIT(5U))
 Secure bit. More...
 
#define ICSSG_FDB_ENTRY_TOUCHED   (ENET_BIT(6U))
 Touched bit. More...
 
#define ICSSG_FDB_ENTRY_VALID   (ENET_BIT(7U))
 Valid bit. More...
 

Typedefs

typedef void(* Icssg_MdioLinkStateChangeCb) (Icssg_MdioLinkStateChangeInfo *info, void *appArg)
 Icssg PHY link state change callback function. More...
 
typedef void(* Icssg_portLinkStateChangeCb) (Enet_MacPort macPort, bool isLinkUp, void *appArg)
 

Enumerations

enum  Icssg_Instance_Num { ICSSG_INSTANCE_NUM_0, ICSSG_INSTANCE_NUM_1, ICSSG_INSTANCE_NUM_2 }
 ICSSG instance numbers. More...
 
enum  Icssg_Ioctl {
  ICSSG_MACPORT_IOCTL_ENABLE_PROMISC_MODE = ICSSG_PUBLIC_IOCTL(0U), ICSSG_MACPORT_IOCTL_DISABLE_PROMISC_MODE = ICSSG_PUBLIC_IOCTL(1U), ICSSG_PER_IOCTL_VLAN_RESET_TABLE = ICSSG_PUBLIC_IOCTL(2U), ICSSG_PER_IOCTL_VLAN_SET_ENTRY = ICSSG_PUBLIC_IOCTL(3U),
  ICSSG_PER_IOCTL_VLAN_GET_ENTRY = ICSSG_PUBLIC_IOCTL(4U), ICSSG_PER_IOCTL_SET_PORT_STATE = ICSSG_PUBLIC_IOCTL(5U), ICSSG_FDB_IOCTL_ADD_ENTRY = ICSSG_PUBLIC_IOCTL(6U), ICSSG_FDB_IOCTL_REMOVE_ENTRY = ICSSG_PUBLIC_IOCTL(7U),
  ICSSG_FDB_IOCTL_REMOVE_ALL_ENTRIES = ICSSG_PUBLIC_IOCTL(8U), ICSSG_FDB_IOCTL_REMOVE_AGEABLE_ENTRIES = ICSSG_PUBLIC_IOCTL(9U), ICSSG_FDB_IOCTL_READ_SLOT_ENTRIES = ICSSG_PUBLIC_IOCTL(10U), ICSSG_FDB_IOCTL_GET_SLOT_ENTRIES = ICSSG_PUBLIC_IOCTL(11U),
  ICSSG_MACPORT_IOCTL_SET_MACADDR = ICSSG_PUBLIC_IOCTL(12U), ICSSG_HOSTPORT_IOCTL_SET_MACADDR = ICSSG_PUBLIC_IOCTL(13U), ICSSG_PER_IOCTL_TAS_TRIGGER = ICSSG_PUBLIC_IOCTL(14U), ICSSG_PER_IOCTL_TAS_ENABLE = ICSSG_PUBLIC_IOCTL(15U),
  ICSSG_PER_IOCTL_TAS_DISABLE = ICSSG_PUBLIC_IOCTL(16U), ICSSG_PER_IOCTL_TAS_RESET = ICSSG_PUBLIC_IOCTL(17U), ICSSG_PER_IOCTL_VLAN_SET_HOSTPORT_DFLT_VID = ICSSG_PUBLIC_IOCTL(18U), ICSSG_PER_IOCTL_VLAN_SET_MACPORT_DFLT_VID = ICSSG_PUBLIC_IOCTL(19U),
  ICSSG_FDB_IOCTL_SET_AGING_PERIOD = ICSSG_PUBLIC_IOCTL(20U), ICSSG_MACPORT_IOCTL_ENABLE_UCAST_FLOOD = ICSSG_PUBLIC_IOCTL(21U), ICSSG_MACPORT_IOCTL_DISABLE_UCAST_FLOOD = ICSSG_PUBLIC_IOCTL(22U), ICSSG_MACPORT_IOCTL_ENABLE_MCAST_FLOOD = ICSSG_PUBLIC_IOCTL(23U),
  ICSSG_MACPORT_IOCTL_DISABLE_MCAST_FLOOD = ICSSG_PUBLIC_IOCTL(24U), ICSSG_MACPORT_IOCTL_SET_ACCEPT_FRAME_CHECK = ICSSG_PUBLIC_IOCTL(25U), ICSSG_MACPORT_IOCTL_SET_INGRESS_RATE_LIM = ICSSG_PUBLIC_IOCTL(26U), ICSSG_MACPORT_IOCTL_SET_QUEUE_CUT_THROUGH_PREEMPT_SELECT = ICSSG_PUBLIC_IOCTL(27U),
  ICSSG_MACPORT_IOCTL_CONFIG_SPL_FRAME_PRIO = ICSSG_PUBLIC_IOCTL(28U), ICSSG_ENABLE_PROTOCOL_SPECIFIC_TAG_IOCTL = ICSSG_PUBLIC_IOCTL(29U), ICSSG_DISABLE_PROTOCOL_SPECIFIC_TAG_IOCTL = ICSSG_PUBLIC_IOCTL(30U), ICSSG_INTERNAL_IOCTL_REGISTER_HANDLER = ICSSG_PUBLIC_IOCTL(31U)
}
 ICSSG IOCTL commands. More...
 
enum  Icssg_QueuePreemptMode { ICSSG_QUEUE_PREEMPT_MODE_EXPRESS, ICSSG_QUEUE_PREEMPT_MODE_PREEMPT }
 Queue preemptive mode: express or preemptive. More...
 
enum  Icssg_QueueForwardMode { ICSSG_QUEUE_FORWARD_MODE_STOREANDFWD, ICSSG_QUEUE_FORWARD_MODE_CUTTHROUGH }
 Queue forward mode: cut-through or store-and-forward. More...
 
enum  Icssg_PortState {
  ICSSG_PORT_STATE_DISABLED, ICSSG_PORT_STATE_BLOCKING, ICSSG_PORT_STATE_FORWARD, ICSSG_PORT_STATE_FORWARD_WO_LEARNING,
  ICSSG_PORT_STATE_TAS_TRIGGER, ICSSG_PORT_STATE_TAS_ENABLE, ICSSG_PORT_STATE_TAS_RESET, ICSSG_PORT_STATE_TAS_DISABLE
}
 Port states. More...
 
enum  Icssg_AcceptFrameCheck { ICSSG_ACCEPT_ONLY_VLAN_TAGGED, ICSSG_ACCEPT_ONLY_UNTAGGED_PRIO_TAGGED, ICSSG_ACCEPT_ALL }
 Acceptable frame check criteria. More...
 

Functions

const Icssg_FwPoolMem * EnetCb_GetFwPoolMem (Enet_Type enetType, uint32_t instId)
 ICSSG memory pool callback function. More...
 
void IcssgMacPort_initCfg (IcssgMacPort_Cfg *macPortCfg)
 Initialises Mac Port COnfiguration. More...
 
uint32_t Icssg_getSliceNum (Enet_Type enetType, uint32_t instId, Enet_MacPort macPort)
 ICSSG memory pool callback function. More...