AM243x MCU+ SDK  12.01.00

Introduction

This module contains APIs to program and use DMA drivers available in the SoC with UART.

Functions

int32_t UART_lld_dmaInit (UARTLLD_Handle hUart, UART_DmaChConfig dmaChCfg)
 API to open an UART DMA channel. More...
 
int32_t UART_lld_dmaDeInit (UARTLLD_Handle hUart)
 API to close an UART DMA channel. More...
 
int32_t UART_lld_dmaWrite (UARTLLD_Handle hUart, const UART_Transaction *transaction)
 API to write data using an UART DMA channel. More...
 
int32_t UART_lld_dmaRead (UARTLLD_Handle hUart, const UART_Transaction *transaction)
 API to read data using an UART DMA channel. More...
 
int32_t UART_lld_dmaDisableChannel (UARTLLD_Handle hUart, uint32_t isChannelTx)
 API to disable DMA channel. More...
 

Function Documentation

◆ UART_lld_dmaInit()

int32_t UART_lld_dmaInit ( UARTLLD_Handle  hUart,
UART_DmaChConfig  dmaChCfg 
)

API to open an UART DMA channel.

This API will open a DMA Channel using the appropriate DMA driver callbacks and the registered via Sysconfig

Parameters
hUart[in] UART Handle
dmaChCfg[in] UART DMA Handle
Returns
SystemP_SUCCESS on success, else failure

◆ UART_lld_dmaDeInit()

int32_t UART_lld_dmaDeInit ( UARTLLD_Handle  hUart)

API to close an UART DMA channel.

Parameters
hUart[in] UART handle returned from UART_open
Returns
SystemP_SUCCESS on success, else failure

◆ UART_lld_dmaWrite()

int32_t UART_lld_dmaWrite ( UARTLLD_Handle  hUart,
const UART_Transaction *  transaction 
)

API to write data using an UART DMA channel.

Parameters
hUart[in] Pointer to UART object
transaction[in] Pointer to UART_Transaction. This parameter can't be NULL
Returns
SystemP_SUCCESS on success, else failure

◆ UART_lld_dmaRead()

int32_t UART_lld_dmaRead ( UARTLLD_Handle  hUart,
const UART_Transaction *  transaction 
)

API to read data using an UART DMA channel.

Parameters
hUart[in] Pointer to UART object
transaction[in] Pointer to UART_Transaction. This parameter can't be NULL
Returns
SystemP_SUCCESS on success, else failure

◆ UART_lld_dmaDisableChannel()

int32_t UART_lld_dmaDisableChannel ( UARTLLD_Handle  hUart,
uint32_t  isChannelTx 
)

API to disable DMA channel.

Parameters
hUart[in] UART Handle
isChannelTx[in] Variable to hold the Tx channel
Returns
SystemP_SUCCESS on success, else failure