AM243x MCU+ SDK  12.01.00
APIs for SDL ECC

Introduction

This Header file contains enumerations, structure definitions and function declarations for SDL ECC interface.

Sub Modules

 ECC_AGGR Data Structures
 
 ECC_AGGR Enumerated Data Types
 
 ECC_AGGR Functions
 
 ECC_AGGR Macros
 
 SDL_ECC_aggrTable
 
 SDL_ECC_memEntries
 

Files

file  sdl_ecc.h
 Header file contains enumerations, structure definitions and function.
 
file  sdl_ecc_soc.h
 Header file contains MemEntries, RamIdTables, aggrTables and aggrBaseAddressTable.
 

Typedefs

typedef void(* SDL_ECC_ErrorCallback_t) (uint32_t errorSrc, uint32_t address)
 
typedef void(* SDL_ECC_VIMDEDVector_t) (void)
 

Typedef Documentation

◆ SDL_ECC_ErrorCallback_t

typedef void(* SDL_ECC_ErrorCallback_t) (uint32_t errorSrc, uint32_t address)

/brief Format of ECC error Call back function

◆ SDL_ECC_VIMDEDVector_t

typedef void(* SDL_ECC_VIMDEDVector_t) (void)

/brief Format of VIM DED vector function

Variable Documentation

◆ SDL_ECC_aggrTransBaseAddressTable

SDL_ecc_aggrRegs* SDL_ECC_aggrTransBaseAddressTable[SDL_ECC_MEMTYPE_MAX]
extern