AM243x MCU+ SDK  12.01.00

Introduction

Data Structures

struct  EnetTas_GenericInArgs
 Generic input args. More...
 
struct  EnetTas_GateCmdEntry
 Gate control list. See IEEE Std 802.1Q-2018 8.6.8.4. More...
 
struct  EnetTas_MaxSDUTable
 Max SDU table. See IEEE Std 802.1Q-2018 12.29.1.1. More...
 
struct  EnetTas_ControlList
 Gate control list. See IEEE Std 802.1Q-2018 8.6.9.4 D3-1. More...
 
struct  EnetTas_ConfigStatus
 Config state machine variables. See IEEE Std 802.1Q-2018 8.6.8.4. More...
 
struct  EnetTas_SetAdminListInArgs
 Input args for ENET_TAS_IOCTL_SET_ADMIN_LIST commands. More...
 
struct  EnetTas_SetStateInArgs
 Input args for ENET_TAS_IOCTL_SET_STATE commands. More...
 

Enumerations

enum  EnetTas_Ioctl {
  ENET_TAS_IOCTL_GET_VERSION = ENET_TAS_PUBLIC_IOCTL(0U), ENET_TAS_IOCTL_SET_ADMIN_LIST = ENET_TAS_PUBLIC_IOCTL(1U), ENET_TAS_IOCTL_GET_OPER_LIST_STATUS = ENET_TAS_PUBLIC_IOCTL(2U), ENET_TAS_IOCTL_SET_STATE = ENET_TAS_PUBLIC_IOCTL(3U),
  ENET_TAS_IOCTL_GET_STATE = ENET_TAS_PUBLIC_IOCTL(4U), ENET_TAS_IOCTL_GET_ADMIN_LIST = ENET_TAS_PUBLIC_IOCTL(5U), ENET_TAS_IOCTL_GET_OPER_LIST = ENET_TAS_PUBLIC_IOCTL(6U), ENET_TAS_IOCTL_CONFIG_CHANGE_STATUS_PARAMS = ENET_TAS_PUBLIC_IOCTL(7U)
}
 TAS module IOCTL commands. More...
 
enum  EnetTas_OperStatus { ENET_TAS_OPER_LIST_NOT_YET_UPDATED = 0, ENET_TAS_OPER_LIST_UPDATED = 1 }
 TAS state types. More...
 
enum  EnetTas_TasState { ENET_TAS_DISABLE = 0, ENET_TAS_ENABLE = 1, ENET_TAS_RESET = 2 }
 TAS state types. More...
 

Macros

#define ENET_TAS_PUBLIC_IOCTL(x)
 Helper macro to create IOCTL commands for TAS module. More...
 
#define ENET_TAS_GATE_MASK(tc7, tc6, tc5, tc4, tc3, tc2, tc1, tc0)
 Helper macro to create a gate mask. More...
 
#define ENET_TAS_MAX_CMD_LISTS   (16)
 Maximum number of gate command entries in each list. More...
 
#define ENET_TAS_MAX_NUM_QUEUES   (8)
 Maximum number of transmit queues supported by implementation. More...
 

Macro Definition Documentation

◆ ENET_TAS_PUBLIC_IOCTL

#define ENET_TAS_PUBLIC_IOCTL (   x)
Value:
ENET_IOCTL_TAS_BASE | \
ENET_IOCTL_MIN(x))

Helper macro to create IOCTL commands for TAS module.

◆ ENET_TAS_GATE_MASK

#define ENET_TAS_GATE_MASK (   tc7,
  tc6,
  tc5,
  tc4,
  tc3,
  tc2,
  tc1,
  tc0 
)
Value:
(((((tc7) != 0U) ? 1U : 0U) << 7U) | \
((((tc6) != 0U) ? 1U : 0U) << 6U) | \
((((tc5) != 0U) ? 1U : 0U) << 5U) | \
((((tc4) != 0U) ? 1U : 0U) << 4U) | \
((((tc3) != 0U) ? 1U : 0U) << 3U) | \
((((tc2) != 0U) ? 1U : 0U) << 2U) | \
((((tc1) != 0U) ? 1U : 0U) << 1U) | \
((((tc0) != 0U) ? 1U : 0U) << 0U))

Helper macro to create a gate mask.

◆ ENET_TAS_MAX_CMD_LISTS

#define ENET_TAS_MAX_CMD_LISTS   (16)

Maximum number of gate command entries in each list.

◆ ENET_TAS_MAX_NUM_QUEUES

#define ENET_TAS_MAX_NUM_QUEUES   (8)

Maximum number of transmit queues supported by implementation.

Enumeration Type Documentation

◆ EnetTas_Ioctl

TAS module IOCTL commands.

Enumerator
ENET_TAS_IOCTL_GET_VERSION 

Get the hardware version of the TAS module.

IOCTL parameters:

Type: Synchronous.

ENET_TAS_IOCTL_SET_ADMIN_LIST 

Set the admin list parameters of the TAS module.

IOCTL parameters:

Type: Asynchronous.

ENET_TAS_IOCTL_GET_OPER_LIST_STATUS 

Get the status of the operational list update.

This IOCTL should be called after ENET_TAS_IOCTL_SET_ADMIN_LIST to verify admin list to operational list copy at specified time. This IOCTL should be called until ENET_TAS_OPER_LIST_UPDATED received as output.

IOCTL parameters:

Type: Synchronous.

ENET_TAS_IOCTL_SET_STATE 

Set the state of the TAS module.

IOCTL parameters:

Type: Asynchronous.

ENET_TAS_IOCTL_GET_STATE 

Get the state of the TAS module.

IOCTL parameters:

Type: Synchronous.

ENET_TAS_IOCTL_GET_ADMIN_LIST 

Get the admin list parameters of the TAS module.

IOCTL parameters:

Type: Synchronous.

ENET_TAS_IOCTL_GET_OPER_LIST 

Get the operational list parameters of the TAS module.

IOCTL parameters:

Type: Synchronous.

ENET_TAS_IOCTL_CONFIG_CHANGE_STATUS_PARAMS 

Get the TAS config change status parameters.

IOCTL parameters:

Type: Synchronous.

◆ EnetTas_OperStatus

TAS state types.

Enumerator
ENET_TAS_OPER_LIST_NOT_YET_UPDATED 

Operational list is not yet updated.

ENET_TAS_OPER_LIST_UPDATED 

Operational list is updated.

◆ EnetTas_TasState

TAS state types.

Enumerator
ENET_TAS_DISABLE 

Idle.

ENET_TAS_ENABLE 

Enable TAS.

ENET_TAS_RESET 

Reset the state machine.

ENET_IOCTL_TYPE_PUBLIC
@ ENET_IOCTL_TYPE_PUBLIC
Definition: enet_ioctl.h:216