AM243x MCU+ SDK  12.01.00

Introduction

Sub Modules

 FreeRTOS Plus CLI Porting Layer
 

Functions

void EnetCli_init (Enet_Type enetType, uint32_t instId)
 Initialize variables necessary for CLI. More...
 
void EnetCli_registerBuiltInCommands ()
 Registers all built-in commands to command interpreter. More...
 
bool EnetCli_processCommand (const char *pCommandInput, char *pWriteBuffer, size_t writeBufferLen)
 Processes the command and runs the associated function. More...
 
const char * EnetCli_getParameter (const char *pCommandString, uint32_t wantedParam, uint32_t *paramLen)
 Extracts a specific parameter from the command. More...
 

Function Documentation

◆ EnetCli_init()

void EnetCli_init ( Enet_Type  enetType,
uint32_t  instId 
)

Initialize variables necessary for CLI.

Gets necessary data like enet handle, core ID and number of MAC ports that are required by the built-in commands.

Parameters
enetTypeEnet peripheral type
instIdEnet peripheral instance ID

◆ EnetCli_registerBuiltInCommands()

void EnetCli_registerBuiltInCommands ( )

Registers all built-in commands to command interpreter.

Use this to enable built-in commands in the application. Should be called only after calling EnetCli_init().

◆ EnetCli_processCommand()

bool EnetCli_processCommand ( const char *  pCommandInput,
char *  pWriteBuffer,
size_t  writeBufferLen 
)

Processes the command and runs the associated function.

Processes the command and executes the function that is associated to the command.

Parameters
pCommandInputThe command to be processed
pWriteBufferBuffer to store output after command is executed
writeBufferLenLength of the output buffer
Returns
true if more data needs to be returned. Otherwise false.

◆ EnetCli_getParameter()

const char* EnetCli_getParameter ( const char *  pCommandString,
uint32_t  wantedParam,
uint32_t *  paramLen 
)

Extracts a specific parameter from the command.

Parameters
pCommandStringThe command from which the parameter needs to be extracted
wantedParamThe parameter index that needs to be extracted
paramLenThe length of the extracted parameter
Returns
A pointer to the first character of the extracted parameter string.