AM243x MCU+ SDK  12.01.00
enet_mod_phy.h File Reference

Introduction

This file contains the type definitions and helper macros for the Ethernet PHY interface.

Go to the source code of this file.

Data Structures

struct  EnetPhy_GenericInArgs
 Generic input args. More...
 
struct  EnetPhy_ReadRegInArgs
 Input args for ENET_PHY_IOCTL_READ_EXT_REG command. More...
 
struct  EnetPhy_WriteRegInArgs
 Input args for ENET_PHY_IOCTL_WRITE_EXT_REG command. More...
 
struct  EnetPhy_C45ReadRegInArgs
 Input args for ENET_PHY_IOCTL_C45_READ_REG command. More...
 
struct  EnetPhy_C45WriteRegInArgs
 Input args for ENET_PHY_IOCTL_C45_WRITE_REG command. More...
 
struct  EnetPhy_PtpPktTimestampInArgs
 Input args for ENET_PHY_IOCTL_GET_PTP_TXTS command. More...
 
struct  EnetPhy_AdjPtpFreqInArgs
 Input args for ENET_PHY_IOCTL_ADJ_PTP_FREQ command. More...
 
struct  EnetPhy_AdjPtpPhaseInArgs
 Input args for ENET_PHY_IOCTL_ADJ_PTP_PHASE command. More...
 
struct  EnetPhy_SetPtpTimeInArgs
 Input args for ENET_PHY_IOCTL_SET_PTP_TIME command. More...
 
struct  EnetPhy_ProcStatusFrameInArgs
 Input args for ENET_PHY_IOCTL_PROC_STATUS_FRAME command. More...
 
struct  EnetPhy_ProcStatusFrameOutArgs
 Output args for ENET_PHY_IOCTL_PROC_STATUS_FRAME command. More...
 
struct  EnetPhy_GetStatusFrameEthdrOutArgs
 Input args for ENET_PHY_IOCTL_GET_STATUS_FRAME_ETHDR command. More...
 
struct  EnetPhy_EnablePtpInArgs
 Input args for ENET_PHY_IOCTL_ENABLE_PTP command. More...
 
struct  EnetPhy_EnableEventCaptureInArgs
 Input args for ENET_PHY_IOCTL_ENABLE_EVENT_CAPTURE command. More...
 
struct  EnetPhy_EnableTriggerOutputInArgs
 Input args for ENET_PHY_IOCTL_ENABLE_TRIGGER_OUTPUT command. More...
 
struct  EnetPhy_GetEventTimestampOutArgs
 Output args for ENET_PHY_IOCTL_GET_EVENT_TIMESTAMP command. More...
 
struct  EnetPhy_ConfigMediaClockInArgs
 Input args for ENET_PHY_IOCTL_CONFIG_MEDIA_CLOCK command. More...
 
struct  EnetPhy_NudgeCodecClockInArgs
 Input args for ENET_PHY_IOCTL_NUDGE_CODEC_CLOCK command. More...
 

Macros

#define ENET_PHY_PUBLIC_IOCTL(x)
 Helper macro to create PHY IOCTL commands. More...
 

Enumerations

enum  EnetPhy_Ioctl_e {
  ENET_PHY_IOCTL_GET_ID = ENET_PHY_PUBLIC_IOCTL(0U), ENET_PHY_IOCTL_GET_SUPPORTED_MODES = ENET_PHY_PUBLIC_IOCTL(1U), ENET_PHY_IOCTL_GET_LOOPBACK_STATE = ENET_PHY_PUBLIC_IOCTL(2U), ENET_PHY_IOCTL_IS_ALIVE = ENET_PHY_PUBLIC_IOCTL(3U),
  ENET_PHY_IOCTL_IS_LINKED = ENET_PHY_PUBLIC_IOCTL(4U), ENET_PHY_IOCTL_GET_LINK_MODE = ENET_PHY_PUBLIC_IOCTL(5U), ENET_PHY_IOCTL_RESET = ENET_PHY_PUBLIC_IOCTL(6U), ENET_PHY_IOCTL_READ_REG = ENET_PHY_PUBLIC_IOCTL(7U),
  ENET_PHY_IOCTL_WRITE_REG = ENET_PHY_PUBLIC_IOCTL(8U), ENET_PHY_IOCTL_READ_EXT_REG = ENET_PHY_PUBLIC_IOCTL(9U), ENET_PHY_IOCTL_WRITE_EXT_REG = ENET_PHY_PUBLIC_IOCTL(10U), ENET_PHY_IOCTL_C45_READ_REG = ENET_PHY_PUBLIC_IOCTL(11U),
  ENET_PHY_IOCTL_C45_WRITE_REG = ENET_PHY_PUBLIC_IOCTL(12U), ENET_PHY_IOCTL_PRINT_REGS = ENET_PHY_PUBLIC_IOCTL(13U), ENET_PHY_IOCTL_ADJ_PTP_FREQ = ENET_PHY_PUBLIC_IOCTL(14U), ENET_PHY_IOCTL_ADJ_PTP_PHASE = ENET_PHY_PUBLIC_IOCTL(15U),
  ENET_PHY_IOCTL_GET_PTP_TIME = ENET_PHY_PUBLIC_IOCTL(16U), ENET_PHY_IOCTL_SET_PTP_TIME = ENET_PHY_PUBLIC_IOCTL(17U), ENET_PHY_IOCTL_GET_PTP_TXTS = ENET_PHY_PUBLIC_IOCTL(18U), ENET_PHY_IOCTL_GET_PTP_RXTS = ENET_PHY_PUBLIC_IOCTL(19U),
  ENET_PHY_IOCTL_WAIT_PTP_TXTS = ENET_PHY_PUBLIC_IOCTL(20U), ENET_PHY_IOCTL_PROC_STATUS_FRAME = ENET_PHY_PUBLIC_IOCTL(21U), ENET_PHY_IOCTL_GET_STATUS_FRAME_ETHDR = ENET_PHY_PUBLIC_IOCTL(22U), ENET_PHY_IOCTL_ENABLE_PTP = ENET_PHY_PUBLIC_IOCTL(23U),
  ENET_PHY_IOCTL_ENABLE_EVENT_CAPTURE = ENET_PHY_PUBLIC_IOCTL(24U), ENET_PHY_IOCTL_ENABLE_TRIGGER_OUTPUT = ENET_PHY_PUBLIC_IOCTL(25U), ENET_PHY_IOCTL_GET_EVENT_TIMESTAMP = ENET_PHY_PUBLIC_IOCTL(26U), ENET_PHY_IOCTL_GET_LINK_STATUS = ENET_PHY_PUBLIC_IOCTL(27U),
  ENET_PHY_IOCTL_CONFIG_MEDIA_CLOCK = ENET_PHY_PUBLIC_IOCTL(28U), ENET_PHY_IOCTL_NUDGE_CODEC_CLOCK = ENET_PHY_PUBLIC_IOCTL(29U)
}
 PHY IOCTL commands. More...
 

Macro Definition Documentation

◆ ENET_PHY_PUBLIC_IOCTL

#define ENET_PHY_PUBLIC_IOCTL (   x)
Value:
ENET_IOCTL_PHY_BASE | \
ENET_IOCTL_MIN(x))

Helper macro to create PHY IOCTL commands.

Enumeration Type Documentation

◆ EnetPhy_Ioctl_e

PHY IOCTL commands.

Enumerator
ENET_PHY_IOCTL_GET_ID 

Get PHY identification.

IOCTL parameters:

ENET_PHY_IOCTL_GET_SUPPORTED_MODES 

Get PHY supported modes by local PHY device.

IOCTL parameters:

ENET_PHY_IOCTL_GET_LOOPBACK_STATE 

Check if PHY is in loopback or not.

IOCTL parameters:

ENET_PHY_IOCTL_IS_ALIVE 

Check PHY alive status.

IOCTL parameters:

ENET_PHY_IOCTL_IS_LINKED 

Check state-machine link state, that is, whether the state machine has reached the LINKED state.

IOCTL parameters:

ENET_PHY_IOCTL_GET_LINK_MODE 

Get the link speed and duplexity state after the state machine has reached the LINKED state.

IOCTL parameters:

ENET_PHY_IOCTL_RESET 

Reset PHY.

IOCTL parameters:

ENET_PHY_IOCTL_READ_REG 

Read PHY register.

IOCTL parameters:

ENET_PHY_IOCTL_WRITE_REG 

Write PHY register.

IOCTL parameters:

ENET_PHY_IOCTL_READ_EXT_REG 

Read PHY extended register.

IOCTL parameters:

ENET_PHY_IOCTL_WRITE_EXT_REG 

Write PHY extended register.

IOCTL parameters:

ENET_PHY_IOCTL_C45_READ_REG 

Read PHY register using Clause-45 frame.

IOCTL parameters:

ENET_PHY_IOCTL_C45_WRITE_REG 

Write PHY register using Clause-45 frame.

IOCTL parameters:

ENET_PHY_IOCTL_PRINT_REGS 

Print PHY registers.

IOCTL parameters:

ENET_PHY_IOCTL_ADJ_PTP_FREQ 

Adjust PHY PTP clock Frequency.

IOCTL parameters:

ENET_PHY_IOCTL_ADJ_PTP_PHASE 

Adjust PHY PTP clock Phase.

IOCTL parameters:

ENET_PHY_IOCTL_GET_PTP_TIME 

Get current PHY PTP clock time.

IOCTL parameters:

ENET_PHY_IOCTL_SET_PTP_TIME 

Set PHY PTP clock time.

IOCTL parameters:

ENET_PHY_IOCTL_GET_PTP_TXTS 

Get PHY PTP TX packet timestamp.

IOCTL parameters:

ENET_PHY_IOCTL_GET_PTP_RXTS 

Get PHY PTP RX packet timestamp.

IOCTL parameters:

ENET_PHY_IOCTL_WAIT_PTP_TXTS 

Add PHY PTP TX packet info to a waiting TX timestamp list.

IOCTL parameters:

ENET_PHY_IOCTL_PROC_STATUS_FRAME 

Process PHY status frame.

IOCTL parameters:

ENET_PHY_IOCTL_GET_STATUS_FRAME_ETHDR 

Get PHY status frame header.

IOCTL parameters:

ENET_PHY_IOCTL_ENABLE_PTP 

Enable/Disable PHY PTP module.

IOCTL parameters:

ENET_PHY_IOCTL_ENABLE_EVENT_CAPTURE 

Enable/Disable an event capture on a PHY GPIO pin.

IOCTL parameters:

ENET_PHY_IOCTL_ENABLE_TRIGGER_OUTPUT 

Enable/Disable clock trigger on a GPIO pin.

IOCTL parameters:

ENET_PHY_IOCTL_GET_EVENT_TIMESTAMP 

Get event timestamp.

IOCTL parameters:

ENET_PHY_IOCTL_GET_LINK_STATUS 

Get Phy Link status. This IOTCL will not have longterm support and this functionality will eventually be merged to ENET_PHY_IOCTL_GET_LINK_MODE IOCTL in upcoming release. So ENET_PHY_IOCTL_GET_LINK_MODE IOCTL can be continued to use to get the phy link speed, duplexity.

IOCTL parameters:

ENET_PHY_IOCTL_CONFIG_MEDIA_CLOCK 

Config Media Clock.

IOCTL parameters:

ENET_PHY_IOCTL_NUDGE_CODEC_CLOCK 

Nudge Codec Clock.

IOCTL parameters:

ENET_IOCTL_TYPE_PUBLIC
@ ENET_IOCTL_TYPE_PUBLIC
Definition: enet_ioctl.h:216