AM243x MCU+ SDK  12.01.00
SYSFW Tools

Note
To see the exact sequence of steps in which boardcfg generation is done, see the makefile inside the ${SDK_INSTALL_PATH}/tools/sysfw/boardcfg/ folder.

Introduction

This section describes the various tools used in conjunction with System Controller Firmware (SYSFW)

Tool requirements on host PC

  • The tools mentioned are implemented using python and needs python version 3.x
  • Refer to the page, Python3 , to install python and the required python packages on your PC.
  • SysConfig tool for using K3 Resource Partitioning Tool: Download SysConfig

Important files and folders

Folder/Files Description
${SDK_INSTALL_PATH}/tools/bin2c/
bin2c.py Tool to convert a binary file to a C array of hexadecimals
${SDK_INSTALL_PATH}/tools/sysfw/boardcfg/
sysfw_boardcfg_validator.py Python script which validates the boardcfg. Used internally in the boardcfg makefile

K3 Resource Partitioning Tool

This tool is based on Texas Instrument's SysConfig tool. It allows you to configure various system level parameters and generate the data which can be fed into many software components. Typical usage for this tool is for System integrators, where one would be able to partition various resources across different software components. These resources includes DMA channels, rings, proxies, interrupts, etc. Apart from this, the tool supports configuration of QoS (Quality of Service) and Firewall parameters which helps in ensuring partitioning of peripheral devices across different CPUs or virtual machines.

Please refer to Modifying resource allocation guide if you want to modify the default resources using K3 Resource Partitioning Tool.

SYSFW Board Config Generation

Note
Please refer to K3 Resource Partitioning Tool section if you want to modify the default resources.

SYSFW Board Config is a SOC specific configuration data regarding the various system attributes controlled by the SYSFW. These include resources, power and clock, security etc. This configuration is sent to SYSFW during boot time. The default configuration is stored in source/drivers/sciclient/sciclient_defaultBoardCfg/{SOC}/

  • Resource Management BoardCfg - sciclient_defaultBoardCfg_rm.c
  • Power Management BoardCfg - sciclient_defaultBoardCfg_pm.c
  • Security BoardCfg - sciclient_defaultBoardCfg_security.c
  • For sending it to SYSFW, these files are converted to hex arrays. We use the bin2c.py python script to do this. This is done internally in the boardcfg makefile. If we change the boardcfg in the above mentioned files, run the following command to generate the hex array header files
make -s -C tools/sysfw/boardcfg sciclient_boardcfg SOC=am243x
  • Once these header files are generated, rebuild the libraries by doing
cd ${SDK_INSTALL_PATH}
gmake -s libs DEVICE={device}
  • After this, make sure to rebuild the secondary bootloader (SBL) applications. You can do this by
cd ${SDK_INSTALL_PATH}
gmake -s sbl DEVICE={device}
  • If you're not using any of the SBLs (SBL UART, SBL OSPI, SBL NULL) and are following the CCS boot method (SOC Initialization Using CCS Scripting), make sure to build the sciclient_ccs_init application by doing
cd ${SDK_INSTALL_PATH}
gmake -s -C examples/drivers/sciclient/sciclient_ccs_init/{board}/r5fss0-0_nortos/ti-arm-clang
Note
This step is only needed if you are using the CCS boot method
  • Once the build is completed, copy the .out file generated and replace with the one already present in ${SDK_INSTALL_PATH}/tools/ccs_load/am243x/ folder.

SYSFW Trace Enable

To enable SYSFW traces, change #undef SYSFW_TRACE_ENABLE to #define SYSFW_TRACE_ENABLE in source/drivers/sciclient/sciclient_default_boardcfg/{SOC}/sciclient_defaultBoardcfg.c. Then rebuild the boardcfg as explained in the above section. This enables all the following trace sources and destinations -

  • Trace Destinations (trace_dst_enables): Controls where logs are output.
    • TISCI_BOARDCFG_TRACE_DST_UART0 - MAIN UART output
    • TISCI_BOARDCFG_TRACE_DST_MEM - Memory buffer
    • TISCI_BOARDCFG_TRACE_DST_ITM - CCS Console
  • Trace Sources (trace_src_enables): Controls which components generate logs
    • TISCI_BOARDCFG_TRACE_SRC_PM - Power Management traces
    • TISCI_BOARDCFG_TRACE_SRC_RM - Resource Management traces
    • TISCI_BOARDCFG_TRACE_SRC_SEC - Security traces
    • TISCI_BOARDCFG_TRACE_SRC_BASE - Baseport traces
    • TISCI_BOARDCFG_TRACE_SRC_USER - User-level traces
    • TISCI_BOARDCFG_TRACE_SRC_SUPR - Supervisor-level traces

Selective Trace Enable

To selectively enable specific traces instead of all, follow these steps:

  1. Locate board configuration file:
    • Path: source/drivers/sciclient/sciclient_default_boardcfg/{SOC}/sciclient_defaultBoardcfg.c
    • Edit the .debug_cfg section in the tisci_boardcfg structure
  2. Configure trace settings based on your needs:

    In the #else block (when SYSFW_TRACE_ENABLE is not defined), replace the default values with your desired configuration:

    Example 1: Enable PM and RM logs to both UART and memory

    Example 2: Enable security logs to UART

  3. Rebuild and reflash board configuration:
    • Follow the instructions in SYSFW Board Config Generation section to regenerate boardcfg
    • Reflash the SBL with the updated board configuration
    • The SYSFW will automatically load the new configuration at runtime

Viewing Trace Output

Depending on the destination flags enabled, logs can be viewed from different locations:

UART Destination (TISCI_BOARDCFG_TRACE_DST_UART0):

  • SYSFW traces are output to MAIN_UART1
    • On Linux host machine, this typically appears as /dev/ttyUSB2
    • Note: The exact USB device number (/dev/ttyUSBx) may vary depending on your EVM configuration and USB connection order. Check dmesg | grep tty after connecting the EVM to identify the correct port.
    • On Windows host machine, use Device Manager to identify the COM port for the MAIN UART
  • Terminal settings: 115200 baud, 8N1 (8 data bits, no parity, 1 stop bit)
  • Recommended tools: minicom, putty, or any serial terminal

Memory Destination (TISCI_BOARDCFG_TRACE_DST_MEM):

ITM Destination (TISCI_BOARDCFG_TRACE_DST_ITM):

  • Logs appear in CCS Console when debugging with Code Composer Studio

SYSFW Trace Parser

After collecting the SYSFW logs as described in the above section, parse them using the sysfw_trace_parser.py script. This will decode the hex trace values and produce a readable text file as output, which helps interpret the logs and debug system issues.

Parsing Trace Logs

  • Run the python script on the Windows command prompt (cmd.exe) or Linux bash shell:
cd ${SDK_INSTALL_PATH}/tools/sysfw/trace_parser
python sysfw_trace_parser.py --log_file <path_to_log_file> --output_file <output_text_file>

Example:

python sysfw_trace_parser.py --log_file sysfw_uart_log.txt --output_file decoded_trace.txt

Getting Help

To view all available command-line options:

python sysfw_trace_parser.py --help

Additional Resources

For more details on trace format and interpretation, refer to: System Firmware Trace Layer Documentation

TISCI_BOARDCFG_TRACE_DST_UART0
#define TISCI_BOARDCFG_TRACE_DST_UART0
Definition: tisci_boardcfg.h:429
TISCI_BOARDCFG_TRACE_DST_MEM
#define TISCI_BOARDCFG_TRACE_DST_MEM
Definition: tisci_boardcfg.h:431
TISCI_BOARDCFG_TRACE_SRC_PM
#define TISCI_BOARDCFG_TRACE_SRC_PM
Definition: tisci_boardcfg.h:455
TISCI_BOARDCFG_TRACE_SRC_RM
#define TISCI_BOARDCFG_TRACE_SRC_RM
Definition: tisci_boardcfg.h:456
TISCI_BOARDCFG_TRACE_SRC_BASE
#define TISCI_BOARDCFG_TRACE_SRC_BASE
Definition: tisci_boardcfg.h:458
TISCI_BOARDCFG_TRACE_SRC_SEC
#define TISCI_BOARDCFG_TRACE_SRC_SEC
Definition: tisci_boardcfg.h:457