AM243x MCU+ SDK  11.01.00

Introduction

This module contains APIs to program and use the OSPI LLD module. The APIs can be used by other drivers to get access to OSPI and also by application to initiate data transfer operation.

Sub Modules

 APIs for OSPI DMA mode
 
 Generic NOR Flash API for single pin mode
 
 Generic Phy layer API.
 
 OSPI Callback Initialization
 
 OSPI Read and Write API's
 
 Transaction Initialization
 
 User Interface API's
 

Files

file  ospi_lld.h
 OSPI LLD Driver API/interface file.
 

Typedefs

typedef void * OSPI_DmaHandle
 The handle for DMA instance used with OSPI. More...
 
typedef void * OSPI_DmaChConfig
 A handle that holds DMA configuration parameters for OSPI. More...
 
typedef void * OSPI_DrvHandle
 

Macros

#define OSPI_RESETPIN_DQ3   (0U)
 
#define OSPI_RESETPIN_DEDICATED   (1U)
 
#define CSL_OSPI_BAUD_RATE_DIVISOR(x)   (((x) - 2U) >> 1U)
 OSPI controller controller mode baud rate divisor. OSPI baud rate = controller_ref_clk/BD, where BD is: 0000 = /2 0001 = /4 0010 = /6 ... 1111 = /32. More...
 
#define MAX_BAUDRATE_DIVIDER   (32U)
 
#define CSL_OSPI_BAUD_RATE_DIVISOR_DEFAULT   (CSL_OSPI_BAUD_RATE_DIVISOR(MAX_BAUDRATE_DIVIDER))
 

Transfer Status Code

Status codes that are set by the OSPI driver

#define OSPI_TRANSFER_COMPLETED   (0U)
 
#define OSPI_TRANSFER_STARTED   (1U)
 
#define OSPI_TRANSFER_CANCELLED   (2U)
 
#define OSPI_TRANSFER_FAILED   (3U)
 
#define OSPI_TRANSFER_CSN_DEASSERT   (4U)
 
#define OSPI_TRANSFER_TIMEOUT   (5U)
 

Transfer Mode

This determines whether the driver operates synchronously or asynchronously

In OSPI_TRANSFER_MODE_BLOCKING OSPI_Transfers block code execution until the transaction has completed

In OSPI_TRANSFER_MODE_CALLBACK OSPI_Transfers does not block code execution and instead calls a callback function when the transaction has completed

#define OSPI_TRANSFER_MODE_BLOCKING   (0U)
 OSPI_Transfers blocks execution. This mode can only be used when called within a Task context and is interrupt based More...
 
#define OSPI_TRANSFER_MODE_CALLBACK   (1U)
 OSPI_Transfers does not block code execution and will call a callback function. This mode can be used in a Task, Swi, or Hwi context More...
 
#define OSPI_TRANSFER_MODE_POLLING   (2U)
 OSPI_Transfers blocks execution. This mode can only be used when called within a Task context and is polling based. More...
 

Frame Format

Definitions for various SPI data frame formats

POL0 = OSPICLK is held low during the INACTIVE state POL1 = OSPICLK is held high during the INACTIVE state

PHA0 = Data launch is on the falling edge of OSPICLK PHA1 = Data launch is on the rising edge of OSPICLK

#define OSPI_FF_POL0_PHA0   (0U)
 
#define OSPI_FF_POL0_PHA1   (CSL_OSPI_FLASH_CFG_CONFIG_REG_SEL_CLK_PHASE_FLD_MASK | 0U)
 
#define OSPI_FF_POL1_PHA0   (0U | CSL_OSPI_FLASH_CFG_CONFIG_REG_SEL_CLK_POL_FLD_MASK)
 
#define OSPI_FF_POL1_PHA1
 

Macros for invalid commands

Macros for invalid commands

#define OSPI_CMD_INVALID_OPCODE   (0xFFU)
 
#define OSPI_CMD_INVALID_DUMMY   (0xFFU)
 
#define OSPI_CMD_INVALID_ADDR   (0xFFFFFFFFU)
 

Macros for command extension types

Macros for command extension types

#define OSPI_CMD_EXT_TYPE_REPEAT   (0x00U)
 
#define OSPI_CMD_EXT_TYPE_INVERSE   (0x01U)
 
#define OSPI_CMD_EXT_TYPE_NONE   (0x02U)
 

Macros for OSPI protocol types

Macros for protocol types

#define OSPI_NOR_PROTOCOL(cmd, addr, data, dtr)
 
#define OSPI_NOR_PROTOCOL_INVALID   (uint32_t)(0xFFFFFFFF)
 
#define OSPI_PROTO_1S_1S_1S   (0x0001)
 
#define OSPI_PROTO_1S_1S_2S   (0x0002)
 
#define OSPI_PROTO_1S_1S_4S   (0x0003)
 
#define OSPI_PROTO_1S_1S_8S   (0x0004)
 
#define OSPI_PROTO_1S_8S_8S   (0x000A)
 
#define OSPI_PROTO_4S_4S_4S   (0x0005)
 
#define OSPI_PROTO_4S_4D_4D   (0x0006)
 
#define OSPI_PROTO_8S_8S_8S   (0x0007)
 
#define OSPI_PROTO_8D_8D_8D   (0x0008)
 
#define OSPI_PROTO_CUSTOM   (0x0009)
 
#define OSPI_NAND_PROTOCOL(cmd, addr, data, dtr)
 
#define OSPI_NAND_PROTOCOL_INVALID   (uint32_t)(0xFFFFFFFF)
 

Chip Selects

Chip selects

#define OSPI_CS0   (0U)
 
#define OSPI_CS1   (1U)
 
#define OSPI_CS2   (2U)
 
#define OSPI_CS3   (3U)
 
#define OSPI_CHIP_SELECT(x)   ((~((1U) << (x))) & 0xFU)
 OSPI Chip select macro. More...
 

Read Mode

Read Mode

#define OSPI_READ_MODE_DAC   (0U)
 
#define OSPI_READ_MODE_INDAC   (1U)
 

Decoder Chip Selects

Decoder Chip selects

#define OSPI_DECODER_SELECT4   ((uint32_t) 0U)
 
#define OSPI_DECODER_SELECT16   ((uint32_t) 1U)
 

Macro Definition Documentation

◆ OSPI_TRANSFER_COMPLETED

#define OSPI_TRANSFER_COMPLETED   (0U)

◆ OSPI_TRANSFER_STARTED

#define OSPI_TRANSFER_STARTED   (1U)

◆ OSPI_TRANSFER_CANCELLED

#define OSPI_TRANSFER_CANCELLED   (2U)

◆ OSPI_TRANSFER_FAILED

#define OSPI_TRANSFER_FAILED   (3U)

◆ OSPI_TRANSFER_CSN_DEASSERT

#define OSPI_TRANSFER_CSN_DEASSERT   (4U)

◆ OSPI_TRANSFER_TIMEOUT

#define OSPI_TRANSFER_TIMEOUT   (5U)

◆ OSPI_TRANSFER_MODE_BLOCKING

#define OSPI_TRANSFER_MODE_BLOCKING   (0U)

OSPI_Transfers blocks execution. This mode can only be used when called within a Task context and is interrupt based

◆ OSPI_TRANSFER_MODE_CALLBACK

#define OSPI_TRANSFER_MODE_CALLBACK   (1U)

OSPI_Transfers does not block code execution and will call a callback function. This mode can be used in a Task, Swi, or Hwi context

◆ OSPI_TRANSFER_MODE_POLLING

#define OSPI_TRANSFER_MODE_POLLING   (2U)

OSPI_Transfers blocks execution. This mode can only be used when called within a Task context and is polling based.

◆ OSPI_FF_POL0_PHA0

#define OSPI_FF_POL0_PHA0   (0U)

◆ OSPI_FF_POL0_PHA1

#define OSPI_FF_POL0_PHA1   (CSL_OSPI_FLASH_CFG_CONFIG_REG_SEL_CLK_PHASE_FLD_MASK | 0U)

◆ OSPI_FF_POL1_PHA0

#define OSPI_FF_POL1_PHA0   (0U | CSL_OSPI_FLASH_CFG_CONFIG_REG_SEL_CLK_POL_FLD_MASK)

◆ OSPI_FF_POL1_PHA1

#define OSPI_FF_POL1_PHA1
Value:
(CSL_OSPI_FLASH_CFG_CONFIG_REG_SEL_CLK_PHASE_FLD_MASK | \
CSL_OSPI_FLASH_CFG_CONFIG_REG_SEL_CLK_POL_FLD_MASK)

◆ OSPI_CMD_INVALID_OPCODE

#define OSPI_CMD_INVALID_OPCODE   (0xFFU)

◆ OSPI_CMD_INVALID_DUMMY

#define OSPI_CMD_INVALID_DUMMY   (0xFFU)

◆ OSPI_CMD_INVALID_ADDR

#define OSPI_CMD_INVALID_ADDR   (0xFFFFFFFFU)

◆ OSPI_CMD_EXT_TYPE_REPEAT

#define OSPI_CMD_EXT_TYPE_REPEAT   (0x00U)

◆ OSPI_CMD_EXT_TYPE_INVERSE

#define OSPI_CMD_EXT_TYPE_INVERSE   (0x01U)

◆ OSPI_CMD_EXT_TYPE_NONE

#define OSPI_CMD_EXT_TYPE_NONE   (0x02U)

◆ OSPI_NOR_PROTOCOL

#define OSPI_NOR_PROTOCOL (   cmd,
  addr,
  data,
  dtr 
)
Value:
(uint32_t)(((uint32_t)(dtr) << 24) | \
((uint32_t)(cmd) << 16) | \
((uint32_t)(addr) << 8) | \
((uint32_t)(data) << 0))

◆ OSPI_NOR_PROTOCOL_INVALID

#define OSPI_NOR_PROTOCOL_INVALID   (uint32_t)(0xFFFFFFFF)

◆ OSPI_PROTO_1S_1S_1S

#define OSPI_PROTO_1S_1S_1S   (0x0001)

◆ OSPI_PROTO_1S_1S_2S

#define OSPI_PROTO_1S_1S_2S   (0x0002)

◆ OSPI_PROTO_1S_1S_4S

#define OSPI_PROTO_1S_1S_4S   (0x0003)

◆ OSPI_PROTO_1S_1S_8S

#define OSPI_PROTO_1S_1S_8S   (0x0004)

◆ OSPI_PROTO_1S_8S_8S

#define OSPI_PROTO_1S_8S_8S   (0x000A)

◆ OSPI_PROTO_4S_4S_4S

#define OSPI_PROTO_4S_4S_4S   (0x0005)

◆ OSPI_PROTO_4S_4D_4D

#define OSPI_PROTO_4S_4D_4D   (0x0006)

◆ OSPI_PROTO_8S_8S_8S

#define OSPI_PROTO_8S_8S_8S   (0x0007)

◆ OSPI_PROTO_8D_8D_8D

#define OSPI_PROTO_8D_8D_8D   (0x0008)

◆ OSPI_PROTO_CUSTOM

#define OSPI_PROTO_CUSTOM   (0x0009)

◆ OSPI_NAND_PROTOCOL

#define OSPI_NAND_PROTOCOL (   cmd,
  addr,
  data,
  dtr 
)
Value:
(uint32_t)(((uint32_t)(dtr) << 24) | \
((uint32_t)(cmd) << 16) | \
((uint32_t)(addr) << 8) | \
((uint32_t)(data) << 0))

◆ OSPI_NAND_PROTOCOL_INVALID

#define OSPI_NAND_PROTOCOL_INVALID   (uint32_t)(0xFFFFFFFF)

◆ OSPI_CS0

#define OSPI_CS0   (0U)

◆ OSPI_CS1

#define OSPI_CS1   (1U)

◆ OSPI_CS2

#define OSPI_CS2   (2U)

◆ OSPI_CS3

#define OSPI_CS3   (3U)

◆ OSPI_CHIP_SELECT

#define OSPI_CHIP_SELECT (   x)    ((~((1U) << (x))) & 0xFU)

OSPI Chip select macro.

◆ OSPI_READ_MODE_DAC

#define OSPI_READ_MODE_DAC   (0U)

◆ OSPI_READ_MODE_INDAC

#define OSPI_READ_MODE_INDAC   (1U)

◆ OSPI_RESETPIN_DQ3

#define OSPI_RESETPIN_DQ3   (0U)

◆ OSPI_RESETPIN_DEDICATED

#define OSPI_RESETPIN_DEDICATED   (1U)

◆ CSL_OSPI_BAUD_RATE_DIVISOR

#define CSL_OSPI_BAUD_RATE_DIVISOR (   x)    (((x) - 2U) >> 1U)

OSPI controller controller mode baud rate divisor. OSPI baud rate = controller_ref_clk/BD, where BD is: 0000 = /2 0001 = /4 0010 = /6 ... 1111 = /32.

◆ MAX_BAUDRATE_DIVIDER

#define MAX_BAUDRATE_DIVIDER   (32U)

◆ CSL_OSPI_BAUD_RATE_DIVISOR_DEFAULT

#define CSL_OSPI_BAUD_RATE_DIVISOR_DEFAULT   (CSL_OSPI_BAUD_RATE_DIVISOR(MAX_BAUDRATE_DIVIDER))

◆ OSPI_DECODER_SELECT4

#define OSPI_DECODER_SELECT4   ((uint32_t) 0U)

◆ OSPI_DECODER_SELECT16

#define OSPI_DECODER_SELECT16   ((uint32_t) 1U)

Typedef Documentation

◆ OSPI_DmaHandle

typedef void* OSPI_DmaHandle

The handle for DMA instance used with OSPI.

◆ OSPI_DmaChConfig

typedef void* OSPI_DmaChConfig

A handle that holds DMA configuration parameters for OSPI.

◆ OSPI_DrvHandle

typedef void* OSPI_DrvHandle
data
uint32_t data
Definition: tisci_rm_psil.h:1
addr
uint64_t addr
Definition: csl_udmap_tr.h:3