Reads the specified thread real-time configuration register from a specified PSI-L thread using the PSI-L configuration proxy. The host requesting the read operation for threads mapped to UDMAP channels must be the owner, or the supervisor of the host owning, the UDMAP channels. For threads not mapped to UDMAP channels, the host requesting the read operation must have access through the region firewall covering the entity to which the thread is mapped. The PSI-L configuration proxy used to read thread's configuration registers is based on the Navigator Subsystem specified by nav_id.
- Parameters
-
hdr | Standard TISCI header |
valid_params | Bitfield defining validity of PSI-L read parameters. This field is unused at the moment but exists if expansion of the API is needed in the future. |
nav_id | SoC device ID of Navigator Subsystem whose PSI-L config proxy is used to read from the thread. |
thread | PSI-L thread ID within the PSI-L System thread map. |
taddr | Thread's configuration register address to read. |