AM243x MCU+ SDK  09.02.01

Detailed Description

A single entry of Processor Access Control List.

Parameters
processor_id- What processor ID are we restricting control over?
proc_access_master- Who is the master who can override control
proc_access_secondary- list of upto PROCESSOR_ACL_SECONDARY_MASTERS_MAX

Data Fields

uint8_t processor_id
 
uint8_t proc_access_master
 
uint8_t proc_access_secondary [PROCESSOR_ACL_SECONDARY_MASTERS_MAX]
 

Field Documentation

◆ processor_id

uint8_t tisci_boardcfg_proc_acl_entry::processor_id

◆ proc_access_master

uint8_t tisci_boardcfg_proc_acl_entry::proc_access_master

◆ proc_access_secondary

uint8_t tisci_boardcfg_proc_acl_entry::proc_access_secondary[PROCESSOR_ACL_SECONDARY_MASTERS_MAX]