AM243x MCU+ SDK  09.02.00
GPMC_nandCmdParams Struct Reference

Detailed Description

Data structure to set NAND command parameters.

Data Fields

uint32_t cmdCycle1
 
uint32_t cmdCycle2
 
uint32_t rowAddress
 
uint32_t numRowAddrCycles
 
uint32_t colAddress
 
uint32_t numColAddrCycles
 
uint32_t waitTimeout
 
uint32_t checkReadypin
 

Field Documentation

◆ cmdCycle1

uint32_t GPMC_nandCmdParams::cmdCycle1

NAND command cycle 1.

◆ cmdCycle2

uint32_t GPMC_nandCmdParams::cmdCycle2

NAND command cycle 2.

◆ rowAddress

uint32_t GPMC_nandCmdParams::rowAddress

NAND row address

◆ numRowAddrCycles

uint32_t GPMC_nandCmdParams::numRowAddrCycles

Number of row address cycles.

◆ colAddress

uint32_t GPMC_nandCmdParams::colAddress

NAND column address.

◆ numColAddrCycles

uint32_t GPMC_nandCmdParams::numColAddrCycles

Number of column address cycles.

◆ waitTimeout

uint32_t GPMC_nandCmdParams::waitTimeout

Wait timeout for the command.

◆ checkReadypin

uint32_t GPMC_nandCmdParams::checkReadypin

Check WAIT PIN status or WAIT PIN interupt status.