AM243x MCU+ SDK  09.02.00
ESM_OpenParams Struct Reference

Detailed Description

ESM Open Parameters.

ESM Open Parameters are used with the ESM_open() call. Default values for these parameters are set using ESM_Params_init().

If NULL is passed for the parameters, ESM_open() uses default parameters.

See also
ESM_Params_init()

Data Fields

Bool bClearErrors
 

Field Documentation

◆ bClearErrors

Bool ESM_OpenParams::bClearErrors

boolean value to indicate if old ESM pending errors should be cleared or not This field will be set by SysCfg. value = 0: do not clear value = 1: clear all ESM group errors