file contains gptp master clock related functions.
Go to the source code of this file.
Functions | |
int | gptpmasterclock_init (const char *shmem_name) |
initialize to get gptp clock from tsn_gptp daemon. if previously initialized, it will simply return 0. More... | |
int | gptpmasterclock_close (void) |
close gptpmasterclcock More... | |
int | gptpmasterclock_gm_domainIndex (void) |
return the domainIndex which is currently used as systeme wide gptp clock. More... | |
int64_t | gptpmasterclock_getts64 (void) |
get 64-bit nsec unit ts of system wide gptp clock More... | |
int | gptpmasterclock_wait_until_ts64 (int64_t tts, int64_t vclose, int64_t toofar) |
Wait until tts comes. More... | |
uint64_t | gptpmasterclock_expand_timestamp (uint32_t timestamp) |
expand 32-bit nsec time to 64 bit with aligning to gptp clock. More... | |
int | gptpmasterclock_gmchange_ind (void) |
get GM change indicator, the number is incremented whenever GM is changed More... | |
int | gptpmasterclock_get_max_domains (void) |
get maximum number of domains More... | |
int | gptpmasterclock_get_domain_ts64 (int64_t *ts64, int domainIndex) |
get a synchronized clock value on specific domain More... | |
void | gptpmasterclock_dump_offset (void) |
print phase offset for all domains More... | |