bindings to TI ENET LLD specific thread, mutex and semaphore functions
Go to the source code of this file.
Typedefs | |
typedef struct cb_lld_sem | cb_lld_sem_t |
typedef struct cb_lld_task | cb_lld_task_t |
Functions | |
int | cb_lld_sem_init (CB_SEM_T *sem, int pshared, unsigned int value) |
Initializes a semaphore. More... | |
int | cb_lld_sem_wait (CB_SEM_T *sem) |
Waits on a semaphore until it becomes available. More... | |
int | cb_lld_sem_trywait (CB_SEM_T *sem) |
Attempts to wait on a semaphore without blocking. To know if the semaphore was acquired, get the return value from the cb_lld_sem_wait_status(). If the return value is 1, then the semaphore was acquired. Otherwise, the semaphore was not acquired. More... | |
int | cb_lld_sem_timedwait (CB_SEM_T *sem, struct timespec *abstime) |
Waits on a semaphore until it becomes available or until a timeout occurs. To know if the semaphore was acquired, refer to the cb_lld_sem_wait_status(). More... | |
int | cb_lld_sem_post (CB_SEM_T *sem) |
Posts (signals) a semaphore, releasing a waiting thread. More... | |
int | cb_lld_sem_getvalue (CB_SEM_T *sem, int *sval) |
return the count of a semaphore More... | |
int | cb_lld_sem_destroy (CB_SEM_T *sem) |
Destroys a semaphore. More... | |
int | cb_lld_sem_wait_status (CB_SEM_T *sem) |
Get the semaphore wait status. The return value of this function determines the wait status of cb_lld_sem_wait(), cb_lld_sem_trywait() and cb_lld_sem_timedwait() More... | |
int | cb_lld_mutex_init (CB_THREAD_MUTEX_T *mutex, CB_THREAD_MUTEXATTR_T attr) |
Initializes a mutex. More... | |
static int | cb_lld_mutex_init_protect (void *mutex) |
Initializes a mutex that will be protected by the ub_protected_func(). More... | |
int | cb_lld_mutex_destroy (CB_THREAD_MUTEX_T *mutex) |
Destroys a mutex. More... | |
int | cb_lld_mutex_lock (CB_THREAD_MUTEX_T *mutex) |
Locks a mutex. More... | |
int | cb_lld_mutex_unlock (CB_THREAD_MUTEX_T *mutex) |
Unlocks a mutex. More... | |
int | cb_lld_mutex_trylock (CB_THREAD_MUTEX_T *mutex) |
Attempts to lock a mutex without blocking. More... | |
int | cb_lld_mutex_timedlock (CB_THREAD_MUTEX_T *mutex, struct timespec *abstime) |
Locks a mutex and waits until a timeout occurs. More... | |
int | cb_lld_task_create (CB_THREAD_T *th, void *attr, void *(*func)(void *), void *arg) |
Creates a new thread. This function creates a new thread with the specified attributes and starts executing the specified function with the provided argument. More... | |
int | cb_lld_task_join (CB_THREAD_T th, void **retval) |
Waits for a thread to terminate. This function waits for the specified thread to terminate. More... | |
void | cb_lld_task_exit (void *retval) |
Terminates the calling thread. More... | |