Bindings to POSIX network functions.
Go to the source code of this file.
Data Structures | |
struct | cb_rawsock_ovip_para_t |
parameters to open the over IP mode raw socket, the values are in host order More... | |
struct | cb_rawsock_paras_t |
raw socket parameters.to open or create raw socket this structure must be filled. More... | |
Macros | |
#define | CB_MAX_NETDEVNAME IFNAMSIZ |
#define | CB_SOCKET_T int |
#define | CB_SOCKET_VALID(x) ((x)>=0) |
#define | CB_SOCKET_INVALID_VALUE -1 |
#define | CB_ETHHDR_T struct ethhdr |
#define | CB_SOCKLEN_T socklen_t |
#define | CB_SOCKADDR_T struct sockaddr |
#define | CB_SOCKADDR_LL_T struct sockaddr_ll |
#define | CB_SOCKADDR_IN_T struct sockaddr_in |
#define | CB_SOCKADDR_IN6_T struct sockaddr_in6 |
#define | CB_SOCKADDR_STORAGE_T struct sockaddr_storage |
#define | CB_IN_ADDR_T struct in_addr |
#define | CB_IN6_ADDR_T struct in6_addr |
#define | CB_IFREQ_T struct ifreq |
#define | CB_OPEN open |
#define | CB_CLOSE close |
#define | CB_WRITE write |
#define | CB_SOCKET socket |
#define | CB_IF_NAMETOINDEX if_nametoindex |
#define | CB_SOCK_BIND bind |
#define | CB_SOCK_IOCTL ioctl |
#define | CB_SOCK_CLOSE close |
#define | CB_SETSOCKOPT setsockopt |
#define | CB_SOCK_SENDTO sendto |
#define | CB_SOCK_RECVFROM recvfrom |
#define | CB_SOCK_RECVMSG recvmsg |
#define | CB_SOCK_WRITE write |
#define | CB_SOCK_CONNECT connect |
#define | CB_FCNTL fcntl |
#define | CB_FD_SET_T fd_set |
#define | CB_FDSET FD_SET |
#define | CB_FDCLR FD_CLR |
#define | CB_FDISSET FD_ISSET |
#define | CB_FDZERO FD_ZERO |
#define | CB_VIRTUAL_ETHDEV_PREFIX "cbeth" |
prefix of virtual network device, which supports raw ethernet packet over udp More... | |
#define | CB_VIRTUAL_PTPDEV_PREFIX "cbptp" |
prefix of virtual ptp device. the suffix must be common with the virtual network device. More... | |
#define | CB_VIRTUAL_ETHDEV_MACU32 {0x02,0x01,0x45,0x10} |
virtual MAC address of the virtual network device. the lower 2 bytes are calculated from the suffix More... | |
#define | H_SOURCE h_source |
#define | H_DEST h_dest |
#define | H_PROTO h_proto |
#define | PTP_HEAD_MSGTYPE(x) ((*(uint8_t *) (&((uint8_t *)(x))[0])) & 0x0F) |
forms ptp header msgtype. More... | |
#define | PTP_HEAD_SEQID(x) ((((uint8_t *)(x))[30]<<8u)|(((uint8_t *)(x))[31])) |
macro which is used to form ptp header sequence id. More... | |
#define | PTP_HEAD_DOMAIN_NUMBER(x) (*(uint8_t *)(&((uint8_t *)(x))[4])) |
macro used to form ptp header domain number. More... | |
#define | MAX_PTPDEV_NAME 32 |
maximum character number of ptp device name More... | |
Typedefs | |
typedef char | ptpdevname_t[MAX_PTPDEV_NAME] |
ptpdevice name. More... | |
typedef char | netdevname_t[CB_MAX_NETDEVNAME] |
network device name. More... | |
Enumerations | |
enum | cb_rawsock_rw_t { CB_RAWSOCK_RDWR = 0, CB_RAWSOCK_RDONLY, CB_RAWSOCK_WRONLY } |
this enumeration defines permission for raw socket. More... | |
enum | cb_sock_mode_t { CB_SOCK_MODE_OVIP = -1, CB_SOCK_MODE_NORMAL } |
Functions | |
int | cb_get_mac_bydev (CB_SOCKET_T sfd, const char *dev, ub_macaddr_t bmac) |
get mac address from device name like 'eth0' More... | |
int | cb_get_ip_bydev (CB_SOCKET_T sfd, const char *dev, CB_IN_ADDR_T *inp) |
get ip address from device name like 'eth0' More... | |
int | cb_get_brdip_bydev (CB_SOCKET_T sfd, const char *dev, CB_IN_ADDR_T *inp) |
get broadcast ip address from device name like 'eth0' More... | |
int | cb_rawsock_open (cb_rawsock_paras_t *llrawp, CB_SOCKET_T *fd, CB_SOCKADDR_LL_T *addr, int *mtusize, ub_macaddr_t bmac) |
generic raw ethernet open More... | |
int | cb_rawsock_close (CB_SOCKET_T fd) |
close the socket opened by cb_rawsock_open More... | |
int | cb_sock_set_priority (CB_SOCKET_T fd, int priority) |
set socket priority More... | |
int | cb_expand_mtusize (CB_SOCKET_T fd, const char *dev, int *mtusize) |
expand mtusize More... | |
int | cb_set_promiscuous_mode (CB_SOCKET_T sfd, const char *dev, bool enable) |
set the promiscuous mode on the socket More... | |
int | cb_reg_multicast_address (CB_SOCKET_T fd, const char *dev, const unsigned char *mcastmac, int del) |
register/deregister multicast address to receive More... | |
int | cb_get_all_netdevs (int maxdevnum, netdevname_t *netdevs) |
get all network devices name availble in systems. More... | |
int | cb_get_ethtool_linkstate (CB_SOCKET_T cfd, const char *dev, uint32_t *linkstate) |
get ethtool link state from device name like 'eth0' More... | |
int | cb_get_ethtool_info (CB_SOCKET_T cfd, const char *dev, uint32_t *speed, uint32_t *duplex) |
get ethtool info(speed and duplex) from device name like 'eth0' More... | |
int | cb_get_netdev_from_ptpdev (char *ptpdev, char *netdev) |
find network device name from ptp device name More... | |
int | cb_get_ptpdev_from_netdev (char *netdev, char *ptpdev) |
find ptp device name from network device name More... | |