AM243x MCU+ SDK  09.00.00

Introduction

UDMA flow related parameters and API.

Go to the source code of this file.

Data Structures

struct  Udma_FlowPrms
 UDMA RX channel flow parameters. More...
 
struct  Udma_FlowAllocMappedPrms
 UDMA RX channel mapped flow alloc parameters. More...
 
struct  Udma_FlowObject
 Opaque UDMA flow object. More...
 

Macros

#define UDMA_DEFAULT_FLOW_ID   (0x3FFFU)
 Default flow ID. More...
 
#define UDMA_FLOW_INVALID   ((uint32_t) 0xFFFF0000U)
 Macro used to specify that flow ID is invalid. More...
 

Functions

int32_t Udma_flowAllocMapped (Udma_DrvHandle drvHandle, Udma_FlowHandle flowHandle, const Udma_FlowAllocMappedPrms *flowAllocMappedPrms)
 UDMA mapped flow allocation API. In devices like AM64x, flows are tied to channels. This API is used to allocate a single flow from the mapped free flows which are dedicated for a particular channel. More...
 
int32_t Udma_flowFree (Udma_FlowHandle flowHandle)
 UDMA free flows. More...
 
int32_t Udma_flowAttach (Udma_DrvHandle drvHandle, Udma_FlowHandle flowHandle, uint32_t flowStart, uint32_t flowCnt)
 UDMA flow attach API. This API is used to attach to an already allocated flow. This API differs from flow alloc API in this aspect - it doesn't allocate resource from RM. Once the flow is attached to, Udma_flowConfig API can be used to configure the flow through sciclient/DMSC API. More...
 
int32_t Udma_flowAttachMapped (Udma_DrvHandle drvHandle, Udma_FlowHandle flowHandle, uint32_t mappepdFlowNum, const Udma_FlowAllocMappedPrms *flowAllocMappedPrms)
 UDMA mapped flow attach API. This API is used to attach to an already allocated mapped flow. This API differs from mapped flow alloc API in this aspect - it doesn't allocate resource from RM. Once the flow is attached to, Udma_flowConfig API can be used to configure the flow through sciclient/DMSC API. More...
 
int32_t Udma_flowDetach (Udma_FlowHandle flowHandle)
 UDMA flow detach API. More...
 
int32_t Udma_flowConfig (Udma_FlowHandle flowHandle, uint32_t flowIdx, const Udma_FlowPrms *flowPrms)
 This API configures the flow configurations. More...
 
uint32_t Udma_flowGetNum (Udma_FlowHandle flowHandle)
 Returns the start flow number managed by this flow handle. More...
 
uint32_t Udma_flowGetCount (Udma_FlowHandle flowHandle)
 Returns the number of flows managed by this flow handle. More...
 
void UdmaFlowPrms_init (Udma_FlowPrms *flowPrms, uint32_t chType)
 Udma_FlowPrms structure init function. More...