AM243x MCU+ SDK  09.00.00
uart_dma.h File Reference

Introduction

UART DMA header file.

Go to the source code of this file.

Data Structures

struct  UART_DmaFxns
 Driver implementation callbacks. More...
 
struct  UART_DmaConfig
 UART DMA Configuration, these are filled by SysCfg based on the DMA driver that is selected. More...
 

Typedefs

typedef void * UART_DmaHandle
 Handle to the UART DMA Config Object returned by UART_dmaOpen. More...
 
typedef int32_t(* UART_dmaOpenFxn) (UART_Handle uartHandle, void *uartDmaArgs)
 Driver implementation to open a specific DMA driver channel - UDMA, EDMA etc. More...
 
typedef int32_t(* UART_dmaTransferReadFxn) (UART_Object *obj, const UART_Attrs *attrs, UART_Transaction *transaction)
 Driver implementation to do a DMA read using a specific DMA driver - UDMA, EDMA etc. More...
 
typedef int32_t(* UART_dmaTransferWriteFxn) (UART_Object *obj, const UART_Attrs *attrs, UART_Transaction *transaction)
 Driver implementation to do a DMA write using a specific DMA driver - UDMA, EDMA etc. More...
 
typedef int32_t(* UART_dmaCloseFxn) (UART_Handle handle)
 Driver implementation to close a specific DMA driver channel - UDMA, EDMA etc. More...
 
typedef int32_t(* UART_dmaDisableChannelFxn) (UART_Handle handle, uint32_t isChannelTx)
 Driver implementation to diisable a specific DMA driver channel - UDMA, EDMA etc. More...
 

Functions

UART_DmaHandle UART_dmaOpen (UART_Handle uartHandle, int32_t index)
 API to open an UART DMA channel. More...
 
int32_t UART_dmaClose (UART_Handle handle)
 API to close an UART DMA channel. More...
 
int32_t UART_dmaDisableChannel (UART_Handle handle, uint32_t isChannelTx)
 API to disable an DMA channel. More...
 
int32_t UART_writeInterruptDma (UART_Object *obj, const UART_Attrs *attrs, UART_Transaction *transaction)
 API to write data using an UART DMA channel. More...
 
int32_t UART_readInterruptDma (UART_Object *obj, const UART_Attrs *attrs, UART_Transaction *transaction)
 API to read data using an UART DMA channel. More...