AM243x MCU+ SDK  09.00.00

Detailed Description

Request message to set keyrev.

This message can only be sent by the host that is tied to root of trust through the secure tisci_boardcfg extended otp extension

Parameters
hdrStandard TISCI header
valueKey Revision value (integer) to be bit encoded, and programmed
cert_addr_loLower 32 bit address (in LE format) of the Dual signed certificate
cert_addr_hiHigher 32 bit address (in LE format) of the Dual signed certificate

Data Fields

struct tisci_header hdr
 
uint32_t value
 
uint32_t cert_addr_lo
 
uint32_t cert_addr_hi
 

Field Documentation

◆ hdr

struct tisci_header tisci_msg_set_keyrev_req::hdr

◆ value

uint32_t tisci_msg_set_keyrev_req::value

◆ cert_addr_lo

uint32_t tisci_msg_set_keyrev_req::cert_addr_lo

◆ cert_addr_hi

uint32_t tisci_msg_set_keyrev_req::cert_addr_hi