Data Fields | |
address_subtype_t | address_subtype |
address_subtype:ipv4, ipv6 More... | |
char | man_address [MAX_ADDRESS_LEN] |
man_address:192.168.88.109 More... | |
bool | tx_enable |
uint32_t | addr_len |
man_addr_if_subtype_t | if_subtype |
uint32_t | if_id |
address_subtype_t management_address_tx_port_t::address_subtype |
address_subtype:ipv4, ipv6
char management_address_tx_port_t::man_address[MAX_ADDRESS_LEN] |
man_address:192.168.88.109
bool management_address_tx_port_t::tx_enable |
uint32_t management_address_tx_port_t::addr_len |
man_addr_if_subtype_t management_address_tx_port_t::if_subtype |
uint32_t management_address_tx_port_t::if_id |