Remote management address info needed.
Data Fields | |
address_subtype_t | address_subtype |
address_subtype:ipv4, ipv6 More... | |
char | address [MAX_ADDRESS_LEN] |
man_address:192.168.88.109 More... | |
man_addr_if_subtype_t | if_subtype |
uint32_t | if_id |
address_subtype_t management_address_t::address_subtype |
address_subtype:ipv4, ipv6
char management_address_t::address[MAX_ADDRESS_LEN] |
man_address:192.168.88.109
man_addr_if_subtype_t management_address_t::if_subtype |
uint32_t management_address_t::if_id |