AM243x MCU+ SDK  09.00.00

Detailed Description

Input parameters for Sciclient_service function.

Data Fields

uint16_t messageType
 
uint32_t flags
 
const uint8_t * pReqPayload
 
uint32_t reqPayloadSize
 
uint32_t timeout
 

Field Documentation

◆ messageType

uint16_t Sciclient_ReqPrm_t::messageType

[IN] Type of message

◆ flags

uint32_t Sciclient_ReqPrm_t::flags

[IN] Flags for messages that are being transmitted.

◆ pReqPayload

const uint8_t* Sciclient_ReqPrm_t::pReqPayload

[IN] Pointer to the payload to be transmitted

◆ reqPayloadSize

uint32_t Sciclient_ReqPrm_t::reqPayloadSize

[IN] Size of the payload to be transmitted (in bytes)

◆ timeout

uint32_t Sciclient_ReqPrm_t::timeout

[IN] Timeout(number of iterations) for receiving response (Refer SystemP_Timeout)