AM243x MCU+ SDK  09.00.00
EnetTimeSync_GetEthTimestampInArgs Struct Reference

Detailed Description

Data Fields

EnetTimeSync_MsgType msgType
 
uint32_t seqId
 
uint32_t portNum
 
uint32_t domain
 

Field Documentation

◆ msgType

EnetTimeSync_MsgType EnetTimeSync_GetEthTimestampInArgs::msgType

TimeSync event message type

◆ seqId

uint32_t EnetTimeSync_GetEthTimestampInArgs::seqId

Sequence id of the event

◆ portNum

uint32_t EnetTimeSync_GetEthTimestampInArgs::portNum

MAC port number corresponding to the event

◆ domain

uint32_t EnetTimeSync_GetEthTimestampInArgs::domain

Domain number of the event