AM243x MCU+ SDK  09.00.00
sdl_rom_checksum.h File Reference

Introduction

This file contains the SDL ROM Checksum API's.

Go to the source code of this file.

Macros

#define SDL_LENGTH_OF_DATA_TO_BE_HASHED   ((uint32_t)196544)
 Macro defines the length of data to be hashed. data to be hashed length is taken from known location of ROM. More...
 
#define SDL_LENGTH_OF_GOLDEN_DATA   ((uint64_t)8)
 Macro defines the length of golden data. Golden data length is taken from known location of ROM. More...
 
#define SDL_GOLDEN_DATA_POINTER   (uint64_t *)(0x004182FFC0)
 Macro defines the pointer of golden data. Golden data pointer is taken from known location of ROM. More...
 
#define SDL_DATA_TO_BE_HASHED_POINTER   (uint8_t *)(0x0041800000)
 Macro defines the pointer of data to be hashed. data to be hashed pointer is taken from known location of ROM. More...
 

Functions

int32_t SDL_ROM_Checksum_compute (void)
 This function will compute Checksum of ROM. More...