![Logo](ti_logo.svg) |
EtherNet/IP™ Adapter3.02.00 |
![](EtherNetIP.png) |
|
◆ EI_API_CIP_getClassAttr()
uint32_t EI_API_CIP_getClassAttr |
( |
T * |
pCipNode_p, |
|
|
uint16_t |
classId_p, |
|
|
EI_API_CIP_SAttr_t * |
pAttr_p |
|
) |
| |
ETHIP_API uint32_t EI_API_CIP_getClassAttr(T *pCipNode_p, uint16_t classId_p, EI_API_CIP_SAttr_t *pAttr_p)
Get class attribute properties.
Definition: EI_API_CIP_stub.c:612
EI_API_CIP_EEdt_t edt
Definition: EI_API_CIP_define.h:189
EI_API_CIP_ECdt_t cdt
Definition: EI_API_CIP_define.h:190
General attribute parameter collection.
Definition: EI_API_CIP_define.h:186
ETHIP_API uint32_t EI_API_CIP_createClass(T *pCipNode_p, uint16_t classId_p)
Create a CIP class.
Definition: EI_API_CIP_stub.c:230
ETHIP_API T * EI_API_CIP_NODE_new(void)
Create a new CIP node.
Definition: EI_API_CIP_stub.c:102
EI_API_CIP_EAr_t accessRule
Definition: EI_API_CIP_define.h:191
uint16_t id
Definition: EI_API_CIP_define.h:188
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_stub.c:256