EtherCAT Slave
1.12.02
◆
EC_API_SLV_getHwVersion()
char* EC_API_SLV_getHwVersion
(
EC_API_SLV_SHandle_t
*
pEcSlaveApi_p
)
Get serial number.
Get serial number. Used by the Object Dictionary
Parameters
[in]
pEcSlaveApi_p
The pointer to the EtherCAT API instance.
Returns
char* Returns the hardware version.
Example
#include <ecSlvApi.h>
EC_API_SLV_SHandle_t
* S_ecSlvApiHdl;
char
* hwVersion = NULL;
// the Call
hwVersion =
EC_API_SLV_getHwVersion
(S_ecSlvApiHdl);
EC_API_SLV_getHwVersion
char * EC_API_SLV_getHwVersion(EC_API_SLV_SHandle_t *pEcSlaveApi_p)
Get serial number.
Definition:
ecSlvApi_ParamStub.c:1051
EC_API_SLV_SHandle_t
struct EC_API_SLV_SHandle EC_API_SLV_SHandle_t
EC_API_SLV_SHandle_t describes the EtherCAT Slave API.
Definition:
ecSlvApi.h:157
See also
EC_API_SLV_setHwVersion
Parameter Configuration
generated by
1.9.1