EtherCAT Slave
1.12.02
◆
EC_API_SLV_cbRegisterPhyReset()
void EC_API_SLV_cbRegisterPhyReset
(
CUST_PHY_CBreset_t
cbFunc_p
,
void *
pContext_p
)
This is the function to register Phy Reset Function.
Parameters
[in]
cbFunc_p
Function pointer to the Phy Reset Handler.
[in]
pContext_p
Call context for PHY Reset.
Example
#include <ecSlvApi.h>
// the Call
retVal =
void
EC_API_SLV_cbRegisterPhyReset
(cbFunc, NULL);
EC_API_SLV_cbRegisterPhyReset
void EC_API_SLV_cbRegisterPhyReset(CUST_PHY_CBreset_t cbFunc_p, void *pContext_p)
This is the function to register Phy Reset Function.
Definition:
ecSlvApi_BoardStub.c:79
Board Support API
generated by
1.9.1