Structure defining Tamagawa command interface.
Firmware command interface
Data Fields | |
volatile uint32_t | word0 |
volatile uint32_t | word1 |
volatile uint32_t tamagawa_cmd::word0 |
command,
[Byte 0] control field
volatile uint32_t tamagawa_cmd::word1 |
command parameters,
[Byte 0] No. of Tx frames
[Byte 1] No. of Rx frames