Struct for MDIO initialization parameters.
Data Fields | |
uint16_t | clkdiv |
uint8_t | addr0 |
uint8_t | addr1 |
uint8_t | link0pol |
uint8_t | link1pol |
uint8_t | enhancedlink_enable |
uint16_t t_mdio_params::clkdiv |
MDIO clkdiv. MDIO clock = 200/(clkdiv+1)
uint8_t t_mdio_params::addr0 |
Address of the PHY hooked to PRU-ICSS MII0
uint8_t t_mdio_params::addr1 |
Address of the PHY hooked to PRU-ICSS MII1
uint8_t t_mdio_params::link0pol |
uint8_t t_mdio_params::link1pol |
uint8_t t_mdio_params::enhancedlink_enable |
Enable enhanced link detection using MII RXLINK and TLK110 enhanced link detection features