TLV2 tag
Data Fields | |
uint8_t | type |
uint8_t | mac_length |
uint8_t | red_mac [ETHER_ADDR_LEN] |
uint8_t TLV2_TAG::type |
Source node identifier set to 30 if the source node is a RedBox
uint8_t TLV2_TAG::mac_length |
Length of the following MAC address in octets
uint8_t TLV2_TAG::red_mac[ETHER_ADDR_LEN] |
MAC addresses used by the RedBox on its interlink