TLV1 tag
Data Fields | |
uint8_t | type |
uint8_t | mac_length |
uint8_t | dan_mac [ETHER_ADDR_LEN] |
uint8_t TLV1_TAG::type |
Indicates the HSR node in normal operation or PRP node in Duplicate Discard or Accept
uint8_t TLV1_TAG::mac_length |
Length of the following MAC address in octets
uint8_t TLV1_TAG::dan_mac[ETHER_ADDR_LEN] |
MAC address used by the sender