Structure defining SDFM thresholds parametrs.
High, Low & zero cross thresholds for sdfm channel
Data Fields | |
volatile uint32_t | high_threshold |
volatile uint32_t | low_threshold |
volatile uint32_t | reserved3 |
volatile uint32_t SDFM_ThresholdParms::high_threshold |
< High threshold value Low threshold value
volatile uint32_t SDFM_ThresholdParms::low_threshold |
reserved for zero crossing
volatile uint32_t SDFM_ThresholdParms::reserved3 |