ICSS EMAC Multicast Filtering Parameters.
Data Fields | |
uint32_t | ctrlOffset |
uint32_t | maskSizeBytes |
uint32_t | maskInitVal |
uint32_t | maskOffset |
uint32_t | overrideStatusOffset |
uint32_t | tableOffset |
uint32_t | ctrlEnabledValue |
uint32_t | ctrlDisabledValue |
uint32_t | maskOverrideSetValue |
uint32_t | maskOverrideNotSetValue |
uint32_t | hostRcvAllowedValue |
uint32_t | hostRcvNotAllowedValue |
uint32_t ICSS_EMAC_FwMulticastFilterParams::ctrlOffset |
uint32_t ICSS_EMAC_FwMulticastFilterParams::maskSizeBytes |
uint32_t ICSS_EMAC_FwMulticastFilterParams::maskInitVal |
uint32_t ICSS_EMAC_FwMulticastFilterParams::maskOffset |
uint32_t ICSS_EMAC_FwMulticastFilterParams::overrideStatusOffset |
uint32_t ICSS_EMAC_FwMulticastFilterParams::tableOffset |
uint32_t ICSS_EMAC_FwMulticastFilterParams::ctrlEnabledValue |
uint32_t ICSS_EMAC_FwMulticastFilterParams::ctrlDisabledValue |
uint32_t ICSS_EMAC_FwMulticastFilterParams::maskOverrideSetValue |
uint32_t ICSS_EMAC_FwMulticastFilterParams::maskOverrideNotSetValue |
uint32_t ICSS_EMAC_FwMulticastFilterParams::hostRcvAllowedValue |
uint32_t ICSS_EMAC_FwMulticastFilterParams::hostRcvNotAllowedValue |