AM243x MCU+ SDK  08.06.00
Cpsw_InterVlanRouteIngressPktMatchCfg Struct Reference

Detailed Description

InterVLAN route ingress packet match criteria configuration.

Data Fields

uint32_t packetMatchEnMask
 
bool ttlCheckEn
 
Enet_MacPort ingressPort
 
CpswAle_MacAddrClassifierInfo srcMacAddrInfo
 
CpswAle_MacAddrClassifierInfo dstMacAddrInfo
 
uint32_t vlanId
 
CpswAle_IpAddrClassifierInfo srcIpInfo
 
CpswAle_IpAddrClassifierInfo dstIpInfo
 
uint16_t etherType
 

Field Documentation

◆ packetMatchEnMask

uint32_t Cpsw_InterVlanRouteIngressPktMatchCfg::packetMatchEnMask

Bitmask selecting classifier types to enable

See also
CPSW Intervlan ingress packet match types

◆ ttlCheckEn

bool Cpsw_InterVlanRouteIngressPktMatchCfg::ttlCheckEn

Flag to enable TTL check. If enabled a packet whose TTL is zero will be routed to host port instead of being routed to egress port

◆ ingressPort

Enet_MacPort Cpsw_InterVlanRouteIngressPktMatchCfg::ingressPort

Port number to match. Must be valid if bit CPSW_INTERVLAN_INGRESSPKT_MATCH_PORT in packetMatchEnMask is set

◆ srcMacAddrInfo

CpswAle_MacAddrClassifierInfo Cpsw_InterVlanRouteIngressPktMatchCfg::srcMacAddrInfo

Source MAC address to match. Must be valid if bit CPSW_INTERVLAN_INGRESSPKT_MATCH_MACSRC in packetMatchEnMask is set

◆ dstMacAddrInfo

CpswAle_MacAddrClassifierInfo Cpsw_InterVlanRouteIngressPktMatchCfg::dstMacAddrInfo

Destination MAC address to match. Must valid if bit CPSW_INTERVLAN_INGRESSPKT_MATCH_MACDST in packetMatchEnMask is set

◆ vlanId

uint32_t Cpsw_InterVlanRouteIngressPktMatchCfg::vlanId

Ingress packet VLAN ID to match

◆ srcIpInfo

CpswAle_IpAddrClassifierInfo Cpsw_InterVlanRouteIngressPktMatchCfg::srcIpInfo

Source IP address to match. Must be valid if bit CPSW_INTERVLAN_INGRESSPKT_MATCH_IPSRC in policerMatchEnMask is set

◆ dstIpInfo

CpswAle_IpAddrClassifierInfo Cpsw_InterVlanRouteIngressPktMatchCfg::dstIpInfo

Destination IP address to match. Must be valid if bit CPSW_INTERVLAN_INGRESSPKT_MATCH_IPDST in policerMatchEnMask is set.

◆ etherType

uint16_t Cpsw_InterVlanRouteIngressPktMatchCfg::etherType

Frame Ethertype to match. Must be valid if bit CPSW_INTERVLAN_INGRESSPKT_MATCH_ETHERTYPE in policerMatchEnMask is set.