Go to the source code of this file.
Macros | |
#define | PNISO_MAX_NUM_EVENTS 2 |
#define | PNISO_MODE_NONE 0 |
#define | PNISO_MODE_INTERRUPT 1 |
#define | PNISO_MODE_GPIO 2 |
#define | PNISO_MODE_DISABLE 0 |
#define | PNISO_MODE_ENABLE 1 |
Typedefs | |
typedef uint32_t * | PNISOM_Handle |
ISOM handle. More... | |
Functions | |
PNISOM_Handle | PN_ISO_initGPIOEvent (PN_Handle pnHandle, uint8_t isoMode, uint32_t timeval, uint32_t duration) |
API to initialize the ISOM event/signal. Returns the ISOM handle. The Event/signal will be disabled by default. More... | |
void | PN_ISO_enableGPIOEvent (PN_Handle pnHandle, PNISOM_Handle isoHandle) |
API to enable the ISOM event/signal generation. More... | |
void | PN_ISO_disableGPIOEvent (PN_Handle pnHandle, PNISOM_Handle isoHandle) |
API to disable the ISOM event/signal generation. More... | |
void | PN_ISO_deInitGPIOEvent (PN_Handle pnHandle, PNISOM_Handle isoHandle) |
API to De init the ISOM event/signal. More... | |
#define PNISO_MAX_NUM_EVENTS 2 |
#define PNISO_MODE_NONE 0 |