Include file for hsrPrp_red_multicastTable.c.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.
Neither the name of Texas Instruments Incorporated nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission.
THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Go to the source code of this file.
Functions | |
RED_STATUS | hsrPrp_multicast_filter_config (PRUICSS_Handle pruicssHandle, uint8_t command) |
set the M_MULTICAST_TABLE_SEARCH_OP_CONTROL_BIT to enable/disable multicast filtering More... | |
RED_STATUS | hsrPrp_multicast_filter_update_macid (PRUICSS_Handle pruicssHandle, uint8_t *multicastAddr, uint8_t command) |
insert/delete a multicast MAC ID in the multicast filter table More... | |
RED_STATUS | hsrPrp_multicast_filter_override_hashmask (PRUICSS_Handle pruicssHandle, uint8_t *mask) |
configure the mask More... | |
RED_STATUS hsrPrp_multicast_filter_config | ( | PRUICSS_Handle | pruicssHandle, |
uint8_t | command | ||
) |
set the M_MULTICAST_TABLE_SEARCH_OP_CONTROL_BIT to enable/disable multicast filtering
pruicssHandle | Handle to PRU ICSS instance. Contains pointers to base addresses & offsets |
command | instruction to enable/disable multicast filtering. Command can take 2 values: MULTICAST_FILTER_DISABLED 0x00 MULTICAST_FILTER_ENABLED 0x01 |
RED_STATUS hsrPrp_multicast_filter_update_macid | ( | PRUICSS_Handle | pruicssHandle, |
uint8_t * | multicastAddr, | ||
uint8_t | command | ||
) |
insert/delete a multicast MAC ID in the multicast filter table
pruicssHandle | Handle to PRU ICSS instance. Contains pointers to base addresses & offsets |
multicastAddr | multicast address to be inserted/deleted into the multicast filter table |
command | instruction to enable/disable multicast filtering. Command can take 2 values: 0 : allow packet to host | ADD_MULTICAST_MAC_ID 1 : do not allow packet to host | REMOVE_MULTICAST_MAC_ID |
RED_STATUS hsrPrp_multicast_filter_override_hashmask | ( | PRUICSS_Handle | pruicssHandle, |
uint8_t * | mask | ||
) |
configure the mask
pruicssHandle | Handle to PRU ICSS instance. Contains pointers to base addresses & offsets |
mask | mask to be set |