Functions | |
int32_t | SDL_RTI_chkWindowSize (uint32_t dwwdWindowSize) |
This API will check the Window Size for DWWD. More... | |
int32_t | SDL_RTI_chkReaction (uint32_t dwwdReaction) |
This API will check the reaction to perform when error is detected from DWWD. More... | |
int32_t | SDL_RTI_getWindowSize (uint32_t baseAddr, uint32_t *pWinSize) |
This API will return current configured Window Size. More... | |
int32_t | SDL_RTI_setPreload (uint32_t baseAddr, uint32_t dwwdPreloadVal) |
Set DWWD preload value. From this value down counter starts down counting. More... | |
int32_t | SDL_RTI_getPreload (uint32_t baseAddr, uint32_t *pPreloadVal) |
This API will return current configured Preload value. More... | |
int32_t SDL_RTI_chkWindowSize | ( | uint32_t | dwwdWindowSize | ) |
This API will check the Window Size for DWWD.
dwwdWindowSize | variable which holds window size which should be verified |
int32_t SDL_RTI_chkReaction | ( | uint32_t | dwwdReaction | ) |
This API will check the reaction to perform when error is detected from DWWD.
dwwdReaction | Variable which holds the reaction to be verified. |
int32_t SDL_RTI_getWindowSize | ( | uint32_t | baseAddr, |
uint32_t * | pWinSize | ||
) |
This API will return current configured Window Size.
baseAddr | Base Address of the RTI instance. |
pWinSize | pointer to Configured Window Size. Refer macro RTI_WindowSize_t |
int32_t SDL_RTI_setPreload | ( | uint32_t | baseAddr, |
uint32_t | dwwdPreloadVal | ||
) |
Set DWWD preload value. From this value down counter starts down counting.
baseAddr | Base Address of the RTI instance. |
dwwdPreloadVal | Down counter preload value. Refer DWWD Down Counter Overview. |
int32_t SDL_RTI_getPreload | ( | uint32_t | baseAddr, |
uint32_t * | pPreloadVal | ||
) |
This API will return current configured Preload value.
baseAddr | Base Address of the RTI instance. |
pPreloadVal | pointer to current preload value |