AM243x MCU+ SDK  08.06.00
APIs for SDL DPL

Introduction

This module contains APIs for using configuring the DPL function pointers to be used by SDL, and also defines the DPL APIs used by SDL for services such as interrupt registration.

Files

file  sdl_dpl.h
 This file contains the SDL DPL API's.
 

Data Structures

struct  SDL_DPL_HwipParams
 This structure contains the parameters for interrupt registration through the SDL DPL interface. More...
 
struct  SDL_DPL_Interface
 This structure contains the pointers for the DPL interfaces provided by the application to SDL_DPL_init. More...
 

Functions

int32_t SDL_DPL_init (SDL_DPL_Interface *dplInterface)
 DPL init. More...
 
int32_t SDL_DPL_enableInterrupt (int32_t intNum)
 DPL enable interrupt. More...
 
int32_t SDL_DPL_disableInterrupt (int32_t intNum)
 DPL disable interrupt. More...
 
int32_t SDL_DPL_registerInterrupt (SDL_DPL_HwipParams *pParams, pSDL_DPL_HwipHandle *handle)
 DPL register interrupt. More...
 
int32_t SDL_DPL_deregisterInterrupt (pSDL_DPL_HwipHandle handle)
 DPL deregister interrupt. More...
 
int32_t SDL_DPL_delay (int32_t ndelay)
 DPL delay. More...
 
void * SDL_DPL_addrTranslate (uint64_t addr, uint32_t size)
 DPL Address translation function. More...
 
int32_t SDL_DPL_globalDisableInterrupts (uintptr_t *key)
 DPL globally disable interrupts. More...
 
int32_t SDL_DPL_globalRestoreInterrupts (uintptr_t key)
 DPL globally enable interrupts. More...
 

Typedefs

typedef void(* pSDL_DPL_InterruptCallbackFunction) (void *arg)
 Prototype for the interrupt callback function. More...
 
typedef void * pSDL_DPL_HwipHandle
 
typedef int32_t(* pSDL_DPL_InterruptFunction) (int32_t intNum)
 Prototype for the interrupt enable/disable functions. More...
 
typedef pSDL_DPL_HwipHandle(* pSDL_DPL_RegisterFunction) (SDL_DPL_HwipParams *pParams)
 Prototype for the interrupt registration function. More...
 
typedef int32_t(* pSDL_DPL_DeregisterFunction) (pSDL_DPL_HwipHandle handle)
 Prototype for the interrupt de-register function. More...
 
typedef int32_t(* pSDL_DPL_DelayFunction) (int32_t ndelay)
 Prototype for the delay function. More...
 
typedef void *(* pSDL_DPL_AddrTranslateFunction) (uint64_t addr, uint32_t size)
 Prototype for address translation function. More...
 
typedef int32_t(* pSDL_DPL_globalDisableInterruptsFunction) (uintptr_t *key)
 Prototype for the interrupt global disable function. More...
 
typedef int32_t(* pSDL_DPL_globalRestoreInterruptsFunction) (uintptr_t key)
 Prototype for the interrupt global restore function. More...
 

Typedef Documentation

◆ pSDL_DPL_InterruptCallbackFunction

typedef void(* pSDL_DPL_InterruptCallbackFunction) (void *arg)

Prototype for the interrupt callback function.

◆ pSDL_DPL_HwipHandle

typedef void* pSDL_DPL_HwipHandle

◆ pSDL_DPL_InterruptFunction

typedef int32_t(* pSDL_DPL_InterruptFunction) (int32_t intNum)

Prototype for the interrupt enable/disable functions.

◆ pSDL_DPL_RegisterFunction

typedef pSDL_DPL_HwipHandle(* pSDL_DPL_RegisterFunction) (SDL_DPL_HwipParams *pParams)

Prototype for the interrupt registration function.

◆ pSDL_DPL_DeregisterFunction

typedef int32_t(* pSDL_DPL_DeregisterFunction) (pSDL_DPL_HwipHandle handle)

Prototype for the interrupt de-register function.

◆ pSDL_DPL_DelayFunction

typedef int32_t(* pSDL_DPL_DelayFunction) (int32_t ndelay)

Prototype for the delay function.

◆ pSDL_DPL_AddrTranslateFunction

typedef void*(* pSDL_DPL_AddrTranslateFunction) (uint64_t addr, uint32_t size)

Prototype for address translation function.

◆ pSDL_DPL_globalDisableInterruptsFunction

typedef int32_t(* pSDL_DPL_globalDisableInterruptsFunction) (uintptr_t *key)

Prototype for the interrupt global disable function.

◆ pSDL_DPL_globalRestoreInterruptsFunction

typedef int32_t(* pSDL_DPL_globalRestoreInterruptsFunction) (uintptr_t key)

Prototype for the interrupt global restore function.

Function Documentation

◆ SDL_DPL_init()

int32_t SDL_DPL_init ( SDL_DPL_Interface dplInterface)

DPL init.

This function initializes the DPL interface structure with the functions provided by the application. These functions are application dependent, so it is required to be passed by the user.

Parameters
dplInterface[IN] DPL interface structure.
Returns
The SDL error code for the API. If dplInterface is NULL: SDL_EBADARGS If other error happened: SDL_EFAIL Success: SDL_PASS

◆ SDL_DPL_enableInterrupt()

int32_t SDL_DPL_enableInterrupt ( int32_t  intNum)

DPL enable interrupt.

This function will enable the specific interrupt number passed.

Parameters
intNum[IN] Interrupt Number
Returns
The SDL error code for the API. If function pointer in interface is NULL: SDL_EBADARGS If other error happened: SDL_EFAIL Success: SDL_PASS

◆ SDL_DPL_disableInterrupt()

int32_t SDL_DPL_disableInterrupt ( int32_t  intNum)

DPL disable interrupt.

This function will disable the specific interrupt number passed.

Parameters
intNum[IN] Interrupt Number
Returns
The SDL error code for the API. If function pointer in interface is NULL: SDL_EBADARGS If other error happened: SDL_EFAIL Success: SDL_PASS

◆ SDL_DPL_registerInterrupt()

int32_t SDL_DPL_registerInterrupt ( SDL_DPL_HwipParams pParams,
pSDL_DPL_HwipHandle handle 
)

DPL register interrupt.

This function will register the specific interrupt number passed.

Parameters
pParams[IN] Parameters for interrupt registration
handle[OUT] Handle for this registered interrupt
Returns
The SDL error code for the API. If function pointer in interface is NULL: SDL_EBADARGS If other error happened: SDL_EFAIL Success: SDL_PASS

◆ SDL_DPL_deregisterInterrupt()

int32_t SDL_DPL_deregisterInterrupt ( pSDL_DPL_HwipHandle  handle)

DPL deregister interrupt.

This function will deregister the specific interrupt number passed.

Parameters
handle[IN] Handle for the registered interrupt
Returns
The SDL error code for the API. If function pointer in interface is NULL: SDL_EBADARGS If other error happened: SDL_EFAIL Success: SDL_PASS

◆ SDL_DPL_delay()

int32_t SDL_DPL_delay ( int32_t  ndelay)

DPL delay.

This function is used assign delay in the function

Parameters
ndelay[IN] delay in microseconds
Returns
The SDL error code for the API. If function pointer in interface is NULL: SDL_EBADARGS If other error happened: SDL_EFAIL Success: SDL_PASS

◆ SDL_DPL_addrTranslate()

void* SDL_DPL_addrTranslate ( uint64_t  addr,
uint32_t  size 
)

DPL Address translation function.

This function is used by the SDL to get a translation for a 64-bit address to local address space. It is expected that the requested adddress will remain available at the returned address and not be removed.

Parameters
addr[IN] Memory address to be translated
size[IN] Size of the memory
Returns
The translated address or (-1) for failure.

◆ SDL_DPL_globalDisableInterrupts()

int32_t SDL_DPL_globalDisableInterrupts ( uintptr_t *  key)

DPL globally disable interrupts.

This function will disable interrupts globally. Interrupts can be enabled with the globalRestoreInterrupts() function. Usually used for critical sections.

The returned key is used to restore the context once interrupts are restored.

Parameters
key[OUT] key to use when restoring interrupts
Returns
The SDL error code for the API. If function pointer in interface is NULL: SDL_EBADARGS If other error happened: SDL_EFAIL Success: SDL_PASS

◆ SDL_DPL_globalRestoreInterrupts()

int32_t SDL_DPL_globalRestoreInterrupts ( uintptr_t  key)

DPL globally enable interrupts.

This function will enable interrupts globally. Usually used for critical sections.

The key is used to restore the context.

Parameters
key[IN] key to use when restoring interrupts
Returns
The SDL error code for the API. If function pointer in interface is NULL: SDL_EBADARGS If other error happened: SDL_EFAIL Success: SDL_PASS