Functions | |
void | HsrFrameFill (hsrPrpHandle *, RED_FRAME *pRedFrame, const uint8_t *pFrame, int32_t frameSize) |
void | HsrFrameUpdatePathId (RED_FRAME *pRedFrame, uint16_t pathId) |
Updates PATH ID of a RED_FRAME. More... | |
RED_FRAME * | HsrSupFrameAllocate (hsrPrpHandle *) |
Allocates a RED_FRAME that holds HSR Supervision frame. More... | |
void | HsrSupFrameUpdateSrcAdd (RED_FRAME *pRedFrame, uint8_t *srcAdd) |
Updates Source Address of a HSR Supervision frame. More... | |
void | HsrSupFrameUpdatePathId (RED_FRAME *pRedFrame, uint16_t pathId) |
void | HsrSupFrameUpdateSeqNr (hsrPrpHandle *, RED_FRAME *pRedFrame) |
void | HsrSupFrameIncrementSeqNr (hsrPrpHandle *) |
void HsrFrameFill | ( | hsrPrpHandle * | , |
RED_FRAME * | pRedFrame, | ||
const uint8_t * | pFrame, | ||
int32_t | frameSize | ||
) |
void HsrFrameUpdatePathId | ( | RED_FRAME * | pRedFrame, |
uint16_t | pathId | ||
) |
RED_FRAME* HsrSupFrameAllocate | ( | hsrPrpHandle * | ) |
void HsrSupFrameUpdateSrcAdd | ( | RED_FRAME * | pRedFrame, |
uint8_t * | srcAdd | ||
) |
Updates Source Address of a HSR Supervision frame.
pRedFrame | pointer to a RED_FRAME |
srcAdd | pointer to a new source address value |
void HsrSupFrameUpdatePathId | ( | RED_FRAME * | pRedFrame, |
uint16_t | pathId | ||
) |
void HsrSupFrameUpdateSeqNr | ( | hsrPrpHandle * | , |
RED_FRAME * | pRedFrame | ||
) |
void HsrSupFrameIncrementSeqNr | ( | hsrPrpHandle * | ) |