Functions | |
void | bsp_set_digio_sw_dataout_enable (PRUICSS_Handle pruIcssHandle) |
Configure digio for sw controlled dataout mode. More... | |
void | bsp_set_digio_out (PRUICSS_Handle pruIcssHandle, uint8_t num) |
Set selected digital output pin. More... | |
void | bsp_clear_digio_out (PRUICSS_Handle pruIcssHandle, uint8_t num) |
Clear selected digital output pin. More... | |
void bsp_set_digio_sw_dataout_enable | ( | PRUICSS_Handle | pruIcssHandle | ) |
Configure digio for sw controlled dataout mode.
pruIcssHandle | PRUSS Handle |
void bsp_set_digio_out | ( | PRUICSS_Handle | pruIcssHandle, |
uint8_t | num | ||
) |
Set selected digital output pin.
pruIcssHandle | PRUSS Handle |
num | digital output selection (num =0 to 7) |
void bsp_clear_digio_out | ( | PRUICSS_Handle | pruIcssHandle, |
uint8_t | num | ||
) |
Clear selected digital output pin.
pruIcssHandle | PRUSS Handle |
num | digital output selection (num =0 to 7) |