AM243x MCU+ SDK  08.06.00

Introduction

Data Structures

struct  EnetQ_Node
 A generic node structure for a single link list. More...
 
struct  EnetQ
 Generic queue. More...
 

Functions

void EnetQueue_initQ (EnetQ *queue)
 Init queue. More...
 
void EnetQueue_copyQ (EnetQ *dstQueue, const EnetQ *srcQueue)
 Copy queues. More...
 
void EnetQueue_enq (EnetQ *queue, EnetQ_Node *node)
 Enqueue a packet into the queue. More...
 
void EnetQueue_enqHead (EnetQ *queue, EnetQ_Node *node)
 Enqueue a packet at head into the queue. More...
 
EnetQ_NodeEnetQueue_deq (EnetQ *queue)
 Dequeue a packet from the queue. More...
 
void EnetQueue_append (EnetQ *dstQueue, EnetQ *srcQueue)
 Append queue. More...
 
uint32_t EnetQueue_getQCount (EnetQ *queue)
 Get queue count. More...
 
void EnetQueue_verifyQCount (EnetQ *queue)
 Checks queue corruption. More...
 

Function Documentation

◆ EnetQueue_initQ()

void EnetQueue_initQ ( EnetQ queue)

Init queue.

Initializes a queue.

Parameters
queueQueue pointer

◆ EnetQueue_copyQ()

void EnetQueue_copyQ ( EnetQ dstQueue,
const EnetQ srcQueue 
)

Copy queues.

Copies queues. The copied queue will have the same head/tail pointers and count as the source queue.

Parameters
dstQueueDestination queue pointer
srcQueueSource queue pointer

◆ EnetQueue_enq()

void EnetQueue_enq ( EnetQ queue,
EnetQ_Node node 
)

Enqueue a packet into the queue.

Enqueues a packet into the queue.

Parameters
queueQueue pointer
nodeQueue node pointer

◆ EnetQueue_enqHead()

void EnetQueue_enqHead ( EnetQ queue,
EnetQ_Node node 
)

Enqueue a packet at head into the queue.

Enqueues a packet into head of queue.

Parameters
queueQueue pointer
nodeQueue node pointer

◆ EnetQueue_deq()

EnetQ_Node* EnetQueue_deq ( EnetQ queue)

Dequeue a packet from the queue.

Dequeues a packet from the queue. A null pointer is returned if the queue was already empty.

Parameters
queueQueue pointer
Returns
Queue node pointer or NULL if queue was empty

◆ EnetQueue_append()

void EnetQueue_append ( EnetQ dstQueue,
EnetQ srcQueue 
)

Append queue.

Appends a packet queue into another queue. The packets in the source queue are queued to the tail of the destination queue.

Parameters
dstQueueDestination queue node pointer
srcQueueSource queue pointer

◆ EnetQueue_getQCount()

uint32_t EnetQueue_getQCount ( EnetQ queue)

Get queue count.

Gets the number of packets in the queue.

Parameters
queueQueue pointer
Returns
Number of packets in the queue

◆ EnetQueue_verifyQCount()

void EnetQueue_verifyQCount ( EnetQ queue)

Checks queue corruption.

Debug API which verifies the queue memory corruption by checking queue count to actual elements in queue. Asserts if queue count doesn't match.

Parameters
queueQueue pointer