AM243x MCU+ SDK  08.06.00
Release Notes 08.03.00

Attention
Also refer to individual module pages for more details on each feature, unsupported features, important usage guidelines.
A53 support is applicable for AM64x only. It is NOT applicable for AM243x.
Note
The examples will show usage of SW modules and APIs on a specific CPU instance and OS combination.
Unless noted otherwise, the SW modules would work in both FreeRTOS and NORTOS environment.
Unless noted otherwise, the SW modules would work on any of the R5F's present on the SOC.
Unless noted otherwise, the SW modules would work on all supported EVMs
All SW modules will not work on M4F. M4F support for a module will be explicitly called out.

New in this Release

Feature Module
32 Task Priority Levels for FreeRTOS Tasks DPL, FreeRTOS
Upgrade to Beckhoff SubDevice Stack Code version 5.13 for EtherCAT examples Industrial Communications Toolkit
PCIe Buffer Transfer between EP and RC modes. Legacy interrupt support. MSI and MSIx capability PCIe
Firewall configuration to enable DMA for secure device DMA
Serial Interface implementation supporting ADS127L11 IC (1.067 MSPS) PRU-IO
Memory footprint optimization in Enet LLD, LWIP, ICSSG ENET, ICSSG, LWIP
Buffered IO boot media support Bootloader
C++ build support and example project added Generic
Added API to check if the interrupt router output is free Sciclient
ICSS based Ethernet, support for DSCP ENET
Enabled combined boot flow (ROM loads SYSFW) Bootloader
SBL Encryption support Bootloader, Security

Device and Validation Information

SOC Supported CPUs Boards Host PC
AM243x R5F, M4F AM243x GP EVM (referred to as am243x-evm in code),
AM243x LAUNCHPAD (referred to as am243x-lp in code)
Windows 10 64b or Ubuntu 18.04 64b

Tools, Compiler and Other Open Source SW Module Information

Tools / SW module Supported CPUs Version
Code Composer Studio R5F, M4F, A53 12.1.0
SysConfig R5F, M4F, A53 1.14.0, build 2667
TI ARM CLANG R5F, M4F 2.1.2.LTS
GCC AARCH64 A53 9.2-2019.12
GCC ARM R5F 7-2017-q4-major (AM64x only)
FreeRTOS Kernel R5F, M4F, A53 10.4.3
FreeRTOS SMP Kernel A53 202110.00-SMP
Tiny USB R5F 0.14.0
LwIP R5F STABLE-2_1_2_RELEASE

Key Features

Experimental Features

Attention
Features listed below are early versions and should be considered as "experimental".
Users can evaluate the feature, however the feature is not fully tested at TI side.
TI would not support these feature on public e2e.
Experimental features will be enabled with limited examples and SW modules.
Feature Module
GUI for UART Uniflash Tool (No support for EMMC flashing) Bootloader

Features not supported in release

  • The ROM startup model for runtime initializations in TI ARM CLANG is not supported/tested in the SDK. We use the RAM model because of the boot-time advantage. For more information on startup models in TI ARM CLANG, refer RAM model v/s ROM model

AM243X LAUNCHPAD not tested/not supported features

Below features are not support on AM243X LAUNCHPAD due to SOC or board constraints,

  • DDR is not supported on the AM243X 11x11 SOC used in AM243X LAUNCHPAD.
  • Motor control examples not validated, due to board limitation
  • I2C temperature sensor example not validated, due to board limitation.
  • M4F examples for UART, MCSPI and GPIO not validated, due to board limitation.

OS Kernel

OS Supported CPUs SysConfig Support Key features tested Key features not tested / NOT supported
FreeRTOS Kernel R5F, M4F, A53 NA Task, Task notification, interrupts, semaphores, mutexes, timers, event groups. ROV views in CCS IDE, Task load measurement using FreeRTOS run time statistics APIs. Only single core A53 FreeRTOS is supported. Second core is NOT used.
FreeRTOS SMP Kernel A53 NA Task, Task notification, interrupts, semaphores, mutexes, timers, event groups. ROV views in CCS IDE, Task load measurement using FreeRTOS run time statistics APIs. -
FreeRTOS POSIX R5F, M4F, A53 NA pthread, mqueue, semaphore, clock -
NO RTOS R5F, M4F, A53 NA See Driver Porting Layer (DPL) below Only single core A53 NORTOS is supported. Second core is NOT used.

Driver Porting Layer (DPL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Address Translate M4F YES FreeRTOS, NORTOS Use RAT to allow M4F access to peripheral address space -
Cache R5F, A53 YES FreeRTOS, NORTOS Cache write back, invalidate, enable/disable -
Clock R5F, M4F, A53 YES FreeRTOS, NORTOS Tick timer at user specified resolution, timeouts and delays -
CpuId R5F NA FreeRTOS, NORTOS Verify Core ID and Cluster ID that application is running -
CycleCounter R5F, M4F, A53 NA FreeRTOS, NORTOS Measure CPU cycles using CPU specific internal counters -
Debug R5F, M4F, A53 YES FreeRTOS, NORTOS Logging and assert to any combo of: UART, CCS, shared memory -
Heap R5F, M4F, A53 NA FreeRTOS, NORTOS Create arbitrary heaps in user defined memory segments -
Hwi R5F, M4F, A53 YES FreeRTOS, NORTOS Interrupt register, enable/disable/restore -
MPU R5F, M4F YES FreeRTOS, NORTOS Setup MPU and control access to address space -
MMU A53 YES NORTOS Setup MMU and control access to address space -
Semaphore R5F, M4F, A53 NA FreeRTOS, NORTOS Binary, Counting Semaphore, recursive mutexs with timeout -
Task R5F, M4F, A53 NA FreeRTOS Create, delete tasks -
Timer R5F, M4F, A53 YES FreeRTOS, NORTOS Configure arbitrary timers -
Event R5F, M4F YES FreeRTOS Setting, getting, clearing, and waiting of Event bits -

Secondary Bootloader (SBL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Bootloader R5FSS0-0 YES NORTOS Boot modes: OSPI, OSPI XIP, UART, SD. All R5F's, M4F, A53 NORTOS/FreeRTOS/Linux boot. RPRC, multi-core image format, DDR init SBL OSPI XIP for A53

SOC Device Drivers

Peripheral Supported CPUs SysConfig Support DMA Supported Key features tested Key features not tested / NOT supported
ADC R5F YES No Single conversion (one-shot mode), interrupt mode, DMA mode Continuous conversion not tested
CRC R5F YES No CRC in full CPU mode -
DDR R5F YES No Tested LPDDR4 at 400MHz frequency. -
ECAP R5F YES No Frequency, Duty cycle, interrupt mode PWM mode not tested
EPWM R5F YES No Different Frequency, Duty cycle, interrupt mode, Deadband and chopper module Tripzone module not tested
EQEP R5F YES No Signal Frequency and Direction, interrupt mode -
FSI (RX/TX) R5F YES No RX, TX, polling, interrupt mode, single/dual lanes -
GPIO R5F, M4F, A53 YES No Basic input/output, GPIO as interrupt GPIO as interrupt is not tested for A53.
GTC R5F, A53 NA No Enable GTC, setting FID (Frequency indicator) -
I2C R5F, M4F, A53 YES No Controller mode, basic read/write, polling and interrupt mode Target mode not supported. M4F not tested due to EVM limitation
IPC Notify R5F, M4F, A53 YES No Low latency IPC between RTOS/NORTOS CPUs -
IPC Rpmsg R5F, M4F, A53 YES No RPMessage protocol based IPC for all R5F, M4F, A53 running NORTOS/FreeRTOS/Linux -
MCAN R5F YES No RX, TX, interrupt and polling mode -
MCSPI R5F, M4F YES Yes Controller/Peripheral mode, basic read/write, polling, interrupt and DMA mode -
MDIO R5F NA No Register read/write, link status and link interrupt enable API -
MMCSD R5F YES Yes Raw read/write and file I/O on MMCSD0 eMMC, and MMCSD1 SD. eMMC tested till HS SDR mode (8-bit data, 52 MHz), SD tested till SD HS mode (4-bit, 25 MHz) Interrupt mode not tested
OSPI R5F YES Yes Read direct, Write indirect, Read/Write commands, DMA for read, PHY Mode Interrupt mode not supported
PCIe R5F YES No Buffer Transfer between EP and RC modes. Legacy interrupt MSI and MSIx capability
Pinmux R5F, M4F, A53 YES No Tested with multiple peripheral pinmuxes -
PRUICSS R5F YES No Tested with Ethercat, EtherNet/IP, IO-Link, ICSS-EMAC, HDSL, EnDat -
SOC R5F, M4F, A53 YES No lock/unlock MMRs, get CPU clock, CPU name, clock enable, set frequency, SW Warm/POR Reset, Address Translation -
Sciclient R5F, M4F, A53 YES No Tested with clock setup, module on/off -
SPINLOCK R5F, M4F, A53 NA No Lock, unlock HW spinlocks -
UART R5F, M4F, A53 YES Yes Basic read/write, polling, interrupt mode, HW flow control not tested. DMA mode not supported
UDMA R5F, A53 YES Yes Basic memory copy, SW trigger, Chaining -
WDT R5F, A53 YES No Interrupt after watchdog expiry Reset not supported

Board Device Drivers

Peripheral Supported CPUs SysConfig Support Key features tested Key features not tested
EEPROM R5F YES I2C based EEPROM -
ETHPHY R5F YES Ethernet Phy configuration for EtherCAT SubDevice example -
Flash R5F YES XSPI, OSPI, QSPI based flash, Octal, Quad mode, DDR mode All vendor flash types not tested
LED R5F, A53 YES GPIO , I2C IO expander based LED control, I2C based industrial LEDs(TPIC2810) -

File System

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
FreeRTOS+FAT R5F YES NORTOS File read, write, create. FAT partition and mounting File I/O with FreeRTOS

CMSIS

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
CMSIS DSP R5F NA FreeRTOS, NORTOS Basic math, complex math, controller, fast math, filtering, Matrix, statistics, transform -

Industrial Communications Toolkit

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
EtherCAT SubDevice FWHAL R5F NO FreeRTOS Tested with ethercat_slave_beckhoff_ssc_demo example Reset isolation
EtherCAT SubDevice Evaluation Stack R5F NO FreeRTOS Tested with ethercat_slave_demo examples -
EtherNet/IP Adapter FWHAL R5F NO FreeRTOS Tested with ethernetip_adapter_demo examples Multicast Filtering
EtherNet/IP Adapter Evaluation Stack R5F NO FreeRTOS Tested with ethernetip_adapter_demo examples -
IO-Link Controller Evaluation Stack R5F NO FreeRTOS Tested with iolink_master_demo example -
Profinet Device FWHAL R5F NO FreeRTOS Tested with profinet_device_demo examples IRT, MRP
Profinet Device Evaluation Stack R5F NO FreeRTOS Tested with profinet_device_demo examples -

Motor Control

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
Position Sense HDSL R5F YES FreeRTOS, NORTOS Freerun mode, Sync mode -
Position Sense EnDAT R5F YES FreeRTOS, NORTOS Single channel, Multi channel, Continuous mode -
Position Sense Tamagawa R5F YES FreeRTOS, NORTOS Absolute position, Encoder ID, Reset -

Networking

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
LwIP R5F YES FreeRTOS TCP/UDP IP networking stack, DHCP, ping, TCP iperf, TCP/UDP IP Other LwIP features, performance and memory optimizations pending, more robustness tests pending
Ethernet driver (ENET) R5F YES FreeRTOS Ethernet as port using CPSW and ICSS, Layer 2 MAC, Layer 2 PTP Timestamping, CPSW Switch -
ICSS-EMAC R5F YES FreeRTOS Tested switch mode with ethernetip_adapter_demo and profinet_device_demo examples EMAC mode, VLAN/Multicast Filtering
ICSS TimeSync R5F NO FreeRTOS Tested E2E mode with ethernetip_adapter_demo examples P2P mode, Transparent Clock mode

USB

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
USB SoC Porting Layer R5F YES FreeRTOS, NORTOS USB 2.0 device mode USB 3.0
USB Device Driver R5F NO FreeRTOS, NORTOS USB 2.0 device mode USB Host driver
TinyUSB Core and CDC Driver R5F NO FreeRTOS, NORTOS USB device with CDC class USB Host, other USB device class drivers

SECURITY

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
SA2UL AES R5F YES NORTOS AES CBC-128 encryption and decryption, AES CBC-256 encryption and decryption, AES ECB-128 encryption and decryption, AES ECB-256 encryption and decryption, AES CMAC-128, AES CMAC-256 -
SA2UL SHA R5F YES NORTOS SHA 512 single shot and multi-shot, SHA 256 single shot and multi-shot, HMAC SHA-256, HMAC SHA-512, HMAC SHA-1 -
SA2UL RNG R5F YES NORTOS RNG generate random number with size of 4 words(128 bit) -
SA2UL PKA R5F YES NORTOS RSA Encryption and Decryption support upto 4k bit, RSA Signing and Verification support upto 4k bit, ECDSA Signing and Verification support with P-256 and P-384 curves -

PRU IO

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
ADS85x8 R5F YES FREERTOS Parallel 8 and 16 Bit Interface with ADS8598H IC OSR Modes, Other ICs

ADS127L11 | R5F | YES | FREERTOS | Serial Interface with ADS127L11 IC | Empty | PRU | NO | Bare Metal | Empty project to get started with PRU firmware development |

Demos

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
Benchmark demo 4xR5F's YES NORTOS CFFT, FIR and FOC benchmarks ADC/PWM benchmark

Fixed Issues

ID Head Line Module Applicable Releases Applicable Devices Resolution/Comments
MCUSDK-3811 Incorrect value for DLR Neighbor Check Interval in EtherNet/IP Adapter FWHAL EtherNet/IP Adapter FWHAL 7.3.0 onwards AM64x, AM243x Fixed
MCUSDK-3644 Removed GCC's objcopy in the boardcfg-gen makefile Build 8.1.0 onwards AM64x, AM243x Fixed
MCUSDK-3558 Secure Boot: DMA based applications fail on HS device SBL SCIClient UDMA 8.2.0 AM64x, AM243x Fixed
MCUSDK-3424 SBL OSPI fails to load image using OSPI DMA in HS device SBL OSPI UDMA 8.2.0 AM64x, AM243x Fixed
MCUSDK-3513 SBL JTAG Example flash write fails if file size is not aligned to multiple of flash page size SBL 8.2.0 AM64x, AM243x Fixed
MCUSDK-3453 Enet: UDMA unable to process icssg rx timestamp and some bytes of packet content after Allocated Packets Enet 8.1.0 onwards AM64x, AM243x Fixed
MCUSDK-2753 SOC_controlModuleLockMMR() doesn't lock CTRLMMR registers Common 8.1.0 onwards AM243x Fixed
MCUSDK-3408 sbl_uart_uniflash write incorrect data to flash due to XMODEM 1024 byte alignment SBL 8.2.0 AM64x, AM243x Fixed
MCUSDK-3398 [SOC]Address translation for R5FSS1 is missing SOC 7.3.0 onwards AM64x, AM243x Fixed
MCUSDK-3712 [FSI]Maximum value of external inputs for triggering frame transmission is limited to 32 SOC 7.3.0 onwards AM64x, AM243x Fixed
MCUSDK-3879 DPL : Inconsistent MPU config for shared memory DPL 7.3.0 onwards AM64x, AM243x Fixed
MCUSDK-3453 Enet ICSSG: UDMA unable to process RX timestamp and packet content while reusing PDs Enet 8.1.0 onwards AM64x, AM243x Fixed
PINDSW-5325 Frame length and frame data is corrupted in MAC mode ENET 8.2.0 AM64x, AM243x Fixed
PINDSW-5315 Zeroing of priority field for 802.1q ingress frames for icssg ENET 8.2.0 AM64x, AM243x Fixed
PINDSW-5318 Switching stalls when traffic is applied to DUT during bootup ENET 8.2.0 AM64x, AM243x Fixed
PINDSW-5280 Higher Cut-through latency and incorrect length(2000 byte) for a smaller packet size(~70 bytes) in 100M/10M link speeds ENET 8.2.0 AM64x, AM243x Fixed
MCUSDK-3947 [MCAN]MCAN message acceptance filter masking is incorrect MCAN 07_03_00 Fixed
MCUSDK-1922 SBL UART appimage size limitation of less then 384 KB SBL 7.3.0 onwards AM64x, AM243x Use the buffered IO implementation of SBL UART
MCUSDK-3325 DDR_VTT_EN is not set by software DDR 8.1.0 onwards AM64x, AM243x -
MCUSDK-3124 AddrTranslateP_setRegion() clears bits in system address above LS 32-bits for R5F RAT DPL 8.2.0 AM64x, AM243x -
MCUSDK-3408 sbl_uart_uniflash writing incorrect data to flash SBL 8.2.0 AM64x, AM243x -
MCUSDK-3424 SBL OSPI fails to load image using OSPI DMA in HS device OSPI, SBL, UDMA 8.2.0 AM64x, AM243x -
MCUSDK-3928 MCU+ SDK board library incorrect condition for while loop BOARD 8.2.0 AM243x -
MCUSDK-4046 Enable I2C in sysconfig to build HDSL diagnostic application if using HDSL-AM64x-E1 Transceiver card HDSL 8.2.0 AM64x -

Known Issues

ID Head Line Module Applicable Releases Applicable Devices Workaround
MCUSDK-626 DMA not working with ADC FIFO 1 ADC 7.3.0 onwards AM64x, AM243x Use ADC FIFO 0
MCUSDK-1016 Semaphore does not function as expected when "post" call is present in multiple ISRs at different priorities DPL 7.3.0 onwards AM64x, AM243x Interrupt nesting should be disabled. SDK disables interrupt nesting by default.
MCUSDK-1900 UART Hardware Flow Control is not working UART 7.3.0 onwards AM243x -
MCUSDK-2113 [Docs] Sysfw RM/PM documentation doesn't specify AM243x Docs 8.0.0 onwards AM243x -
MCUSDK-2135 Insufficient UDMA TX channels allocated for Dual-mac mode Enet 8.1.0 onwards AM64x, AM243x Allocate minimum of 2 TX channels(ENET_CFG_TX_CHANNELS_NUM macro) in enet_cfg.h file
MCUSDK-2319 2 PRU(ICSS) driver instances are added while changing Enet ICSSG instance to ICSSG0 in SysConfig SYSCFG 8.1.0 onwards AM64x, AM243x Please remove the extra one manually
MCUSDK-2409 MCRC CRCSetPSASeedSig() API sets channel mode to DATA capture CRC 8.1.0 onwards AM64x
MCUSDK-2419 MCSPI TX Only mode is not functional in DMA mode MCSPI, UDMA 8.2.0 onwards AM64x, AM243x Use TX/RX mode and ignore RX.
MCUSDK-2715 PKA ECDSA sign verify is not working for P-521 and BrainPool P-512R1 curves SECURITY 8.2.0 onwards AM64x, AM243x -
MCUSDK-3626 Enet: Phy tuning is not done correctly on AM64x/AM243x and AM263x platforms Enet 8.1.0 onwards AM64x, AM243x PHY delay is not tuned but set to value based on limited testing on a small set of boards.If packet drops are still seen, we can force the phy to set to 100mbps.Make below change in application code: linkCfg->speed = ENET_SPEED_100MBIT; linkCfg->duplexity = ENET_DUPLEX_FULL;
MCUSDK-4080 DDR_init call after warm reset causes crash in System in OSPI mode DDR 8.2.0 AM64x, AM243x DDR_init should not be called in SBL if DDR is already initialized
MCUSDK-4379 Low Tx side throughput seen when tested using iperf application DDR 8.3.0 AM64x, AM243x -
MCUSDK-4379 Low Tx side throughput seen when tested using iperf application INDUS_PROTOCOL_HSR_PRP 8.3.0 AM64x, AM243x

Replace mcu_plus_sdk\source\networking\lwip\lwip-config\am243x\lwipopts.h and mcu_plus_sdk\source\networking\lwip\lwip-config\am243x\lwippools.h from MCU PLUS SDK 8.2.0 release and rebuild lwip_freertos, lwip-contrib and icss_emac_lwip_if libraries.

Limitations

ID Head Line Module Reported in Release Applicable Devices Workaround
MCUSDK-208 gmake with -j can sometimes lock up Windows command prompt Build 7.3.0 AM64x, AM243x Use bash for windows as part of git for windows or don't use -j option

Upgrade and Compatibility Information

Attention
When migrating from Processor SDK RTOS, see Migration Guides for more details

This section lists changes which could affect user applications developed using older SDK versions. Read this carefully to see if you need to do any changes in your existing application when migrating to this SDK version relative to previous SDK version. Also refer to older SDK version release notes to see changes in earlier SDKs.

Compiler Options

Module Affected API Change Additional Remarks

Examples

Module Affected API Change Additional Remarks

OS Kernel

Module Affected API Change Additional Remarks

SOC Device Drivers

Module Affected API Change

Additional Remarks

Sysconfig Sysconfig G5 and F5 pin data In AM243 LP Sysconfig data file the G5 pin was incrrectly assigned to F5 which is fixed now and G5 is not a valid pin now

For AM243 LP any application using G5 pin earlier should use F5 pin in Sysconfig now

Industrial Communications Toolkit

Module Affected API Change Additional Remarks
EtherCAT SubDevice FWHAL bsp_init Added new parameter phy_rx_err_reg in bsp_params Allows configuration of vendor specific 0x0E28 register in TI EtherCAT SubDevice Controller (ESC) for the RX Error counting during frames.