This structure is used for the Scan Status List of a single scan result. More...
#include <IOLM_SMI_Types.h>
Data Fields | |
INT16U | u16ArgBlockID |
Big endian. | |
INT8U | u8ScanStatus |
Scan status. | |
INT8U | u8ScanResults |
Number of scan results (max 255). | |
IOLM_SMI_SScanStatusResult | asResult [1] |
array of scan results | |
This structure is used for the Scan Status List of a single scan result.
The ArgBlockID(IOLM_SMI_EArgBlockID) for this struct is IOLM_SMI_eArgBlockID_WScanStatusList = 0x9201.