This structure is used to store wireless port configuration. More...
#include <IOLM_SMI_Types.h>
Data Fields | |
INT16U | u16ArgBlockID |
Big endian. | |
INT8U | u8PortMode |
INT8U | u8ValidationBackup |
INT8U | u8IQBehavior |
INT8U | u8PortCycleTime |
INT16U | u16VendorID |
Big endian. | |
INT32U | u32DeviceID |
Big endian. | |
INT8U | u8Slot |
slot number starting with 0 | |
INT8U | u8Track |
track number starting with 1 | |
INT8U | u8DeviceTxPower |
INT8U | u8MaxRetry |
INT8U | u8ImaTimeBase |
Time Base 0x01 - 0x04. More... | |
INT8U | u8ImaTimeMulti |
Big endian 0x01 - 0xFF. More... | |
INT8U | u8SlotType |
0 = SSLOT / 1 = DSLOT. | |
INT8U | u8LowPowerDevice |
0 = Normal Device / 1 = Low Power. | |
INT8U | u8MaxPDSegLength |
INT8U | u8WMasterCycleTimePDOut |
INT8U | u8WMasterCycleTimePDIn |
INT8U | au8UniqueID [9] |
This structure is used to store wireless port configuration.
The ArgBlockID(IOLM_SMI_EArgBlockID) for this struct is IOLM_SMI_eArgBlockID_WPortConfigList = 0x8002.
INT8U IOLM_SMI_SWPortConfigList::u8ImaTimeBase |
Time Base 0x01 - 0x04.
<
INT8U IOLM_SMI_SWPortConfigList::u8ImaTimeMulti |
Big endian 0x01 - 0xFF.
<