This structure is used for SPDU input. More...
#include <IOLM_SMI_Types.h>
Data Fields | |
INT16U | u16ArgBlockID |
Big endian. | |
INT8U | au8Data [32] |
32 bytes. | |
This structure is used for SPDU input.
The ArgBlockID(IOLM_SMI_EArgBlockID) for this struct is IOLM_SMI_eArgBlockID_SPDUIn = 0x1101.