This structure is used to store FS port status. More...
#include <IOLM_SMI_Types.h>
Data Fields | |
INT16U | u16ArgBlockID |
Big endian. | |
INT8U | u8PortStatusInfo |
IOLM_SMI_EPortStatus. | |
INT8U | u8PortQualityInfo |
INT8U | u8RevisionID |
INT8U | u8TransmissionRate |
INT8U | u8MasterCycleTime |
INT8U | u8InputDataLength |
INT8U | u8OutputDataLength |
INT16U | u16VendorID |
Big endian. | |
INT32U | u32DeviceID |
Big endian. | |
INT8U | u8NumberOfDiags |
INT8U | au8DiagData [3 *5] |
This structure is used to store FS port status.
The ArgBlockID(IOLM_SMI_EArgBlockID) for this struct is IOLM_SMI_eArgBlockID_FSPortStatusList = 0x9100.