This structure is used to store FS port configuration. More...
#include <IOLM_SMI_Types.h>
Data Fields | |
INT16U | u16ArgBlockID |
Big endian. | |
INT8U | u8PortMode |
INT8U | u8ValidationBackup |
INT8U | u8IQBehavior |
INT8U | u8PortCycleTime |
INT16U | u16VendorID |
Big endian. | |
INT32U | u32DeviceID |
Big endian. | |
INT16U | u16FSPTime2Ready |
INT32U | u32FSCPAuthenticity1 |
INT32U | u32FSCPAuthenticity2 |
INT8U | u8FSPPort |
INT16U | u16FSPAuthentCRC |
INT8U | u8FSPProtVersion |
INT8U | u8FSPProtMode |
INT16U | u16FSPWatchdogTime |
INT16U | u16FSPIOStructCRC |
INT32U | u32FSPTechParCRC |
INT16U | u16FSPProtParCRC |
INT8U | u8IODescVersion |
INT8U | u8SPDUInLength |
INT8U | u8TotalOfInBits |
INT8U | u8TotalOfInOctets |
INT8U | u8TotalOfInInt16 |
INT8U | u8TotalOfInInt32 |
INT8U | u8SPDUOutLength |
INT8U | u8TotalOfOutBits |
INT8U | u8TotalOfOutOctets |
INT8U | u8TotalOfOutInt16 |
INT8U | u8TotalOfOutInt32 |
This structure is used to store FS port configuration.
The ArgBlockID(IOLM_SMI_EArgBlockID) for this struct is IOLM_SMI_eArgBlockID_FSPortConfigList = 0x8100.