#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
errCode =
EI_API_ADP_setIpConfig(pEI_API_ADP, configurationControl, 0xC0A8010A, 0xFFFFFF00, 0xC0A80101, 0x0, 0x0,
"",
false);
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:301
ETHIP_API uint32_t EI_API_ADP_setIpConfig(T *pAdp_p, EIP_SConfigurationControl_t configurationControl_p, uint32_t ipAddr_p, uint32_t netwMask_p, uint32_t gateway_p, uint32_t nameServer1_p, uint32_t nameServer2_p, char *pDomainName_p, bool applyChanges)
Set the IP configuration of the selected adapter (Instance Attribute ID: 3 and 5).
Definition: EI_API_ADP_main.c:3452
EIP_EConfigurationMethod_t configurationMethod
Definition: EI_API_ADP.h:234
bool dnsEnable
Definition: EI_API_ADP.h:235
uint32_t reserved
Definition: EI_API_ADP.h:236
Definition: EI_API_ADP.h:233