#include <api/EI_API.h>
uint32_t errCode;
tParam.pruInstance = CONFIG_PRU_ICSS1;
tParam.phy0Instance = CONFIG_ETHPHY0;
tParam.phy1Instance = CONFIG_ETHPHY1;
ETHIP_API void EI_API_ADP_pruicssStart(void)
Starts the PRU0 and PRU1 firmware on the PRU-ICSS block instance specified in EI_API_ADP_pruicssInit.
Definition: EI_API_ADP_main.c:201
ETHIP_API uint32_t EI_API_ADP_pruicssInit(EIP_SLoadParameter *ptPara_p)
Load and initialize the EtherNet/IP firmware in the PRU.
Definition: EI_API_ADP_main.c:107
uint8_t ai8uMacAddr[EIP_MAC_ADDR_LEN]
Definition: EI_API_ADP.h:178
Definition: EI_API_ADP.h:177